License expired for S32 Design Studio for S32 Platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License expired for S32 Design Studio for S32 Platform

Jump to solution
450 Views
HSchill
Contributor I

Hi,
My License have expiered  jul 29

Activation code: B61B-2364-2E5B-C7EE

Can you pls extend it ?

Regards 
Hans

0 Kudos
Reply
1 Solution
429 Views
stanish
NXP Employee
NXP Employee

Hello Hans,

Indeed, the license to the package SW32G-STDSW-D has already expired. Since this is a common activation code for all alpha users issued 4 years ago, I'd strongly recommend to re-activate the license using the activation code from your personal NXP account.  The activation code allows to be used on 100 devices so you should be able to activate and use the package on another machine. (I noticed it was so far activated just once)

Your personal account activation code starts with 2949-F4xx-xxxx-xxxx

Please send me a private message if there is any issue related to activation code so I can assist you more.

 

Hope it helps.

Stan

 

 

View solution in original post

0 Kudos
Reply
1 Reply
430 Views
stanish
NXP Employee
NXP Employee

Hello Hans,

Indeed, the license to the package SW32G-STDSW-D has already expired. Since this is a common activation code for all alpha users issued 4 years ago, I'd strongly recommend to re-activate the license using the activation code from your personal NXP account.  The activation code allows to be used on 100 devices so you should be able to activate and use the package on another machine. (I noticed it was so far activated just once)

Your personal account activation code starts with 2949-F4xx-xxxx-xxxx

Please send me a private message if there is any issue related to activation code so I can assist you more.

 

Hope it helps.

Stan

 

 

0 Kudos
Reply