KEA SDK in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA SDK in S32DS

1,788件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

In CW v11, it can be created project with PEx(processor expert) for KEA but it can't be in S32DS. I created a project with KEAZN64 sdk, but it can't be used PEx. Could you guide about how to use PEx for KEA? 

Should I use CW v11 only? Or create and use the project with PEx in CW v11 and then it can be imported to S32DS? 

Also, can I get an example code with PEx for KEA? 

FYI, I'm using KEAZN16. 

Best regards,

Kate Lee

ラベル(2)
0 件の賞賛
返信
1 返信

1,680件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Kate,

I'm affraid PEx is not supported by S32DS for KEA.  The only SDK available in S32DS is Example grade set of low level drivers (.c, *.h). PEx project created in CodeWarrior cannot be imported by S32DS - it is not compatible.

If you intend on using PEx + KEA then use CodeWarrior or alternativelly KDS if it's still available.

Regards,

Stan

0 件の賞賛
返信