KEA SDK in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA SDK in S32DS

1,837 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

In CW v11, it can be created project with PEx(processor expert) for KEA but it can't be in S32DS. I created a project with KEAZN64 sdk, but it can't be used PEx. Could you guide about how to use PEx for KEA? 

Should I use CW v11 only? Or create and use the project with PEx in CW v11 and then it can be imported to S32DS? 

Also, can I get an example code with PEx for KEA? 

FYI, I'm using KEAZN16. 

Best regards,

Kate Lee

Labels (2)
0 Kudos
Reply
1 Reply

1,729 Views
stanish
NXP Employee
NXP Employee

Hi Kate,

I'm affraid PEx is not supported by S32DS for KEA.  The only SDK available in S32DS is Example grade set of low level drivers (.c, *.h). PEx project created in CodeWarrior cannot be imported by S32DS - it is not compatible.

If you intend on using PEx + KEA then use CodeWarrior or alternativelly KDS if it's still available.

Regards,

Stan

0 Kudos
Reply