Is it possible to replace ARM GCC toolchain by IAR toolchain for ARM in S32 DS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to replace ARM GCC toolchain by IAR toolchain for ARM in S32 DS?

1,806 Views
samerbastawy
Contributor I

PS: I have the IAR license but I want to switch from building my project using ARM GCC, to IAR. Any suggestions?

Labels (1)
Tags (3)
1 Reply

1,528 Views
stanish
NXP Employee
NXP Employee

Hi Samer,

S32DS for ARM supports IAR eclipse plugin. This allows you to create and build the project with IAR Toolchain and also debug it using IAR C-SPY debug engine under S32DS Eclipse environment.

For more information about how to install and use IAR plugin see the post below:

https://community.nxp.com/thread/438558?commentID=931340#comment-851981 

Hope it helps.

Stan