Installing S32DS 3.4 on Ubuntu 18.04 has trouble.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing S32DS 3.4 on Ubuntu 18.04 has trouble.

1,318件の閲覧回数
davidNad
Contributor I

I saw the 'S32DS_Installation Guide_3.4.0.pdf' and finished installing it.

But when I run S32DS, I get the following log :

 

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.ram.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.ram.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.lib.

Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.lib.

2022-10-04 16:52:20.452:INFO:oeju.TypeUtil:qtp273821181-42: JVM Runtime does not support Modules
WebKit wasn't able to find a WebVTT encoder. Not continuing without platform support for subtitles.

 

 

 

And if i create S32DS application project, I get the following log :

 

(S32 Design Studio:15306): Gtk-WARNING **: 16:52:36.206: gtk_widget_size_allocate(): attempt to allocate widget with width 12 and height -13

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:36.206: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.909: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.909: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.913: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.915: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.916: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.924: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar

(S32 Design Studio:15306): Gtk-CRITICAL **: 16:52:48.924: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar
Warning: NLS unused message: ImportSdkRenameDialog_SAME_NAME in: com.nxp.s32ds.cle.cdt.sdk.internal.ui.messages
Warning: NLS unused message: SDKManifestProvider_37 in: com.nxp.s32ds.cle.uct.core.messages
Warning: NLS missing message: SDKManifest_OverwriteFiles in: com.nxp.s32ds.cle.uct.core.messages
WARNING: | Thrown Exception: No valid yaml sections found [PreparedImportStatus.preparePrjImport]
com.nxp.swtools.provider.importer.YamlNotFoundException: No valid yaml sections found
at com.nxp.swtools.utils.scripting.YamlConverter.parse(YamlConverter.java:144)
at com.nxp.swtools.periphs.controller.importer.PeriphsImporter.parse(PeriphsImporter.java:105) ...
SEVERE: [SDK] Importer.parser failed: board/Siul2_Port_Ip_Cfg.c [PreparedImportStatus.preparePrjImport]
WARNING: | Thrown Exception: No valid yaml sections found [PreparedImportStatus.preparePrjImport]
com.nxp.swtools.provider.importer.YamlNotFoundException: No valid yaml sections found
at com.nxp.swtools.utils.scripting.YamlConverter.parse(YamlConverter.java:144)
at com.nxp.swtools.periphs.controller.importer.PeriphsImporter.parse(PeriphsImporter.java:105) ...
SEVERE: [SDK] Toolchain project import failed: No YAML found in `board/Clock_Ip_Cfg.c` [ImportToolchainProjectFactory.logError4User]

 

And when i do something like 'Open Pins', I get a lot of warning logs.

Theses are examples of one of them

 

WARNING: USDHC_CLK: missing output group type. Peripheral will be used instead. [ClockSignalInterface.<init>]
WARNING: USDHC0_CLK: missing output group type. Peripheral will be used instead. [ClockSignalInterface.<init>]
WARNING: WKPU0_CLK: missing output group type. Peripheral will be used instead. [ClockSignalInterface.<init>]
WARNING: 'description' shall not be empty in register[PORTLOLSR].bit_field[LOLF0].bit_field_value[PORTLOLSR_LOLF0_LOSS_LOCK_NO] in file /home/NXP/S32DS.3.4/eclipse/mcu_data/processors/S32G274A_Rev2/PlatformSDK_S32G_2020_12/S32G274A_Rev2_525bga/registers/PERIPH_DFS.xml [DatabaseXmlLoader.logProblem]
WARNING: 'description' shall not be empty in register[PORTLOLSR].bit_field[LOLF0].bit_field_value[PORTLOLSR_LOLF0_LOSS_LOCK_YES] in file /home/NXP/S32DS.3.4/eclipse/mcu_data/processors/S32G274A_Rev2/PlatformSDK_S32G_2020_12/S32G274A_Rev2_525bga/registers/PERIPH_DFS.xml [DatabaseXmlLoader.logProblem]

 

And when I click 'Open Peripehrals - Components - + button(Driver)' , the following message apperas. But I need a Siul2_Dio driver.

 

SEVERE: Could not find any matching component for type Siul2_Dio [AddComponentDialog.filterComponents]
SEVERE: Could not find any matching component for type Stm [AddComponentDialog.filterComponents]
SEVERE: Could not find any matching component for type Ctu_Ip [AddComponentDialog.filterComponents]
SEVERE: Could not find any matching component for type Wkpu [AddComponentDialog.filterComponents]
SEVERE: Could not find any matching component for type XRDC [AddComponentDialog.filterComponents]

 

Could you let me know how I can install S32DS 3.4 properly?

 

0 件の賞賛
返信
1 返信

1,294件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

it looks that you probably missed some dependency. Please check again if you installed all requested libraries (32bits/64bits) - even the optional ones. 

0 件の賞賛
返信