Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installation of S32DS.3.4_b201217_win32.x86_64 rolling back

1,822 Views
bvikas
NXP Employee
NXP Employee

Installation of S32SD3.4 is not completing. It is rolling back before asking for Activation code.

Please find attached the logs.

Thanks

0 Kudos
Reply
8 Replies

1,774 Views
bvikas
NXP Employee
NXP Employee

Hi All,

We need to get Local Admin rights to install S32 Design Studion V-3.4 and V3.5

0 Kudos
Reply

1,806 Views
bvikas
NXP Employee
NXP Employee

I am running as Admin
But still the same issue.

0 Kudos
Reply

1,792 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

As an NXP employee, please start 'Admin by Request' session AND use the 'Run as Administrator' option from the right-click menu on the installer. It seems sometimes the admin status is not functioning as expected and this procedure has worked for some NXP users.

Best Regards,

Mike

0 Kudos
Reply

1,775 Views
bvikas
NXP Employee
NXP Employee

Hello Mike,

These steps are also not working.

0 Kudos
Reply

1,748 Views
mikedoidge
NXP Employee
NXP Employee

Hello @bvikas,

We recently discussed the issue with NXP IT. They recommend using the option 'Windows 7 compatibility mode' when installing S32 Design Studio to avoid the admin rights issue. Please try this and let us know if it resolves your issue.

Best Regards,

Mike

0 Kudos
Reply

1,770 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I think you need to contact IT, please submit a SNOW ticket to get this resolved. It could be the access setup for your account on your PC which are different in some way to cause you more difficulty than other NXP users.

Mike

0 Kudos
Reply

1,813 Views
hanraaijmakers
NXP Employee
NXP Employee

run as admin

0 Kudos
Reply

1,814 Views
hanraaijmakers
NXP Employee
NXP Employee

We have the same problem.

0 Kudos
Reply