Install IAR Eclipse plug-in into S32 Design Studio for ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install IAR Eclipse plug-in into S32 Design Studio for ARM

2,434 Views
347996379
Contributor III

hello. 

I want to use IAR compiler. so I install IAR Plugin manager that following this "HOWTO_Install_IAR_Eclipse_plugin_into_S32_Design_Studio_for_ARM.pdf"

But I encountered the following problem during installation.

Cap 2019-05-13 10-37-43-284.png

After installation, I did check 'window->preferences'. but there is no 'IAR Embedded Workbench'

Cap 2019-05-13 10-38-19-784.png

->I run IAR plugin manager (Menu "Help" -> "IAR Embedded Workbench plugin manager...") , can show the below info. 

pastedImage_1.png

Note: I already installed IAR workbench in my laptop, the path is C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4\,  the version is 8.42.1

 

-> after click the "Install" button into next step. 

pastedImage_1.png

-> select all, and click the "Next"  button:

pastedImage_2.png

-> click the "Next"  button, problem is occurred, installation failed.  

pastedImage_3.png

  • What is the problem? Could you help me analyze the reason?

Tags (2)
0 Kudos
Reply
2 Replies

1,871 Views
turgaykale
Contributor III

I am facing with the same problem, is there any solution ?

0 Kudos
Reply

2,239 Views
chaitanya_kalyani
Contributor III

Hello,

 

I am also facing same issue. Have you find any solution for this. 

0 Kudos
Reply