sir please send me the link to download SDK RTM 3.0.0 and how to add to the S32DS and configure it.
You can download it from: S32DS-ARM: S32 Design Studio for Arm
Here you can refer how to add to the S32DS: S32 Design Studio for ARM 2018.R1 - Update 11 available
You can know more from: S32DS for ARM - list of HOWTOs
Best Regards,
Robin
Hi Veeraju,
For S32K1xx, the recommended SDK version to use is S32K1xx SDK RTM3.0.0 with UP10(SR3.0.1) and 11(SR3.0.2) installed;
Then you can refer the example in SDK
Then you can find the "Start_here.html" in it's folder:
You may need to read "examples and demos" and "Modules"
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Give explanation about recive and transmit operation with SDK function