I just download S32 design studio but can't import an existing project. Do I need license or activation code?

cancel
Showing results for 
Search instead for 
Did you mean: 

I just download S32 design studio but can't import an existing project. Do I need license or activation code?

398 Views
Contributor I

While importing a project and reach the project folder with the project shown but greyed out, the project can not be selected and move to next to complete the import.

0 Kudos
3 Replies

31 Views
NXP Employee
NXP Employee

Hi, 

which version of S32DS are you using (ARM, PowerPC, Vision?)

When you already installed S32DS - your license code is okay. Is the project which you are trying to import the old S32DS project?

Jiri

0 Kudos

31 Views
Contributor I

I have the version 2017.R1 and I am importing an old project. So do I need to re-setup a new project?

0 Kudos

31 Views
NXP Employee
NXP Employee

Hi, 

here is old project migration guide - HOWTO: Migrate project created in S32DS Power v1.x into v1.2+ 

Jiri

0 Kudos