How to use Jlink on S32DS3.5 to perform all operations on S32K144 on-chip FLASH

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use Jlink on S32DS3.5 to perform all operations on S32K144 on-chip FLASH

跳至解决方案
1,402 次查看
SethWang
NXP Employee
NXP Employee

Hi

    I am using S32DS3.5, and I want to use Jlink to erase all the on-chip FLASH of S32K144, but I can’t find the option to realize this function on the interface of S32DS3.5. How should I do it?

    In addition, I would like to know, to use Jlink to download a project, is it to erase all the on-chip FLASH of S32K144? Or only erase the FLASH of the size required by the actual project? thank you~

0 项奖励
回复
1 解答
1,371 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually - in S32DS is not Erase only option available. If you are flashing new project - the full erase is performed prior to flashing project binary. Hope it answers both questions.  

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,372 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually - in S32DS is not Erase only option available. If you are flashing new project - the full erase is performed prior to flashing project binary. Hope it answers both questions.  

0 项奖励
回复