How to support the S32K11x in S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to support the S32K11x in S32 Design Studio

1,579件の閲覧回数
xch0520
Contributor I

I am using the S32K116 and S32K118 to develop my product. The S32 Design Studio for ARM V2.0 has been installed, in which I can't find the S32K118 when the new project was created. Where I can find the device package for S32K118? I've found the device packge for S32K116 in NXP's website, but the K118 can't be found.

Besides, I've also tried to install the S32 Design Studio for ARM 2018.R1. It can't support the S32K11x series MCU defaultly. The update packages in NXP's website are too complex to let my know which one I need to install, would you give me some advice?

Miller Xue

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,423件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately only S32K116 is supported by older S32DS for Arm v2.0. S32DS for Arm v2018.R1 needs to be updated for full S32K1xx support - https://community.nxp.com/docs/DOC-341068

Hope it helps. 

Jiri 

0 件の賞賛
返信

1,423件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

S32DS 2.0 does not support S32K116 and S32K118. These are supported in S32DS 2018.R1. But you also need to install the newest update.

Please see the link below. As soon as you install this update, you can create project for every S32K1xx microcontroller.

Here is link for downloading S32DS 2018.R1 for ARM

S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! 

Here is link for update

https://community.nxp.com/docs/DOC-343020 

Regards,

Martin

0 件の賞賛
返信