How to specify the size of enum type variables in S32DS3.4 for S32K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to specify the size of enum type variables in S32DS3.4 for S32K

跳至解决方案
2,760 次查看
jinjingyang
NXP Employee
NXP Employee

Dear sir,

Customer want to have all enum type variables with size of uint32 type.

But S32DS will set all enum to its minimum size.

If the max value of a enum variable is less than 255, its size will be 1 byte.

But customer want that all enum variables be 32bit size.

How can we configure this compiler option?

I have tried to remove the optimization option "-fshort-enums" but it doesn't work.

Could you please provide some possible methods? 

0 项奖励
回复
1 解答
2,749 次查看
jinjingyang
NXP Employee
NXP Employee

I just found that the compiler option "-fno-short_enums" can be used to resovle this issue.

With this option, the enum type will be 32bit size.

By default, the option "-fshort_enums" is used, which will use minimum size for enums.

So please close this topic.

在原帖中查看解决方案

1 回复
2,750 次查看
jinjingyang
NXP Employee
NXP Employee

I just found that the compiler option "-fno-short_enums" can be used to resovle this issue.

With this option, the enum type will be 32bit size.

By default, the option "-fshort_enums" is used, which will use minimum size for enums.

So please close this topic.