How to setup PFE driver in s32g274a

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to setup PFE driver in s32g274a

3,565 次查看
yihan_cheng
Contributor II

Hi 

I have downloaded the PFE Firmware file class_s32g.elf. But I don't know how to setup it.

In the user manuel said:

The fi rmware binary available on the target either in the le system or built into the driver depending on which driver is being used.

I copy class_s32g.elf to the root filesystem from my board in /lib/firmware/, however when i boot the EVB

PFEng firmware file 'mmc@0:1:pfe-s32g-class.fw' loading failed: -2

Thanks and Greeting

Yihan

0 项奖励
回复
2 回复数

3,431 次查看
athul_pk
Contributor I

Hello ,

I do have the same problem.

I have the bsp and yocto recipes for PFE . but from where I will get class_s32g.elf

Thanks in advance

0 项奖励
回复

3,431 次查看
yihan_cheng
Contributor II

Hi,

I find the solution, there are bsp image with the PFE driver included. Beside it, you can use yocto to convert .elf to .bin

only the .bin files will work in linux image.

BR

Yihan Cheng

0 项奖励
回复