How to setup PFE driver in s32g274a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to setup PFE driver in s32g274a

3,479 Views
yihan_cheng
Contributor II

Hi 

I have downloaded the PFE Firmware file class_s32g.elf. But I don't know how to setup it.

In the user manuel said:

The fi rmware binary available on the target either in the le system or built into the driver depending on which driver is being used.

I copy class_s32g.elf to the root filesystem from my board in /lib/firmware/, however when i boot the EVB

PFEng firmware file 'mmc@0:1:pfe-s32g-class.fw' loading failed: -2

Thanks and Greeting

Yihan

0 Kudos
Reply
2 Replies

3,345 Views
athul_pk
Contributor I

Hello ,

I do have the same problem.

I have the bsp and yocto recipes for PFE . but from where I will get class_s32g.elf

Thanks in advance

0 Kudos
Reply

3,345 Views
yihan_cheng
Contributor II

Hi,

I find the solution, there are bsp image with the PFE driver included. Beside it, you can use yocto to convert .elf to .bin

only the .bin files will work in linux image.

BR

Yihan Cheng

0 Kudos
Reply