How to set the format of Motorola S-Record in S32DS(ARM v2.2)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to set the format of Motorola S-Record in S32DS(ARM v2.2)?

跳至解决方案
2,194 次查看
ManManXiang
Contributor II

When I set to generate S-record file in S32DS the record format  in S-Record file was only 'S1' for all lines.

Please see below:

S1130000007000201104000059040000590400008D
S113001059040000590400005904000000000000C5
S1130020000000000000000000000000590400006F
S11300305904000000000000590400004DCB0000EA
S1130040A7480000B5480000C3480000D14800009C
S1130050DF480000ED480000FB48000009490000AB
S113006017490000254900003349000041490000B8
S11300704F4900005D4900006B49000079490000C8
S11300808749000059040000590400005904000085
S113009059040000590400005904000059040000E8
S11300A05904000059040000E79A0000F59A000082
S11300B0039B000059040000590400005904000087
S11300C059040000590400005904000059040000B8
S11300D059040000590400005904000059040000A8
S11300E05904000059040000590400005904000098
S11300F05904000059040000590400005904000088
S11301005904000059040000590400005904000077
S11301105904000059040000590400005904000067
S11301205904000059040000590400005904000057
S11301305904000059040000590400005904000047
S11301405904000059040000590400005904000037
S11301505904000059040000590400005904000027
 
How or where can I set the format to 'S2' or 'S3' ? Please help me!
标记 (1)
0 项奖励
回复
1 解答
2,187 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 项奖励
回复
2 回复数
2,188 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

please take a look at this thread:

https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1234442

Regards,

Lukas

0 项奖励
回复
2,174 次查看
ManManXiang
Contributor II

Thanks!The problem was successfully solved.

0 项奖励
回复