How to run the project on S32 ds with openSDA and Devkit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run the project on S32 ds with openSDA and Devkit?

1,593 次查看
1506840872
Contributor II

Hey, everyone. I bought a Devkit-MPC5744P recently and download the S32 design studio from the NXP website. It is OK to build an example project and debug the project with the openSDA to the devkit .

But when I click the "RUN" button, problem always occur:

lauching *.elf has encountered a problem ; error Starting Process.

1.jpg

"Step into " and "step over"  are available .But the project cannot be run.

I just wanna know how to run the project, thank you.

0 项奖励
回复
1 回复

1,411 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

please use Debug button (one icon left next to the RUN button) instead of RUN button. The run button is not implemented.

Regards,

Martin

0 项奖励
回复