Hello Community,
Currently I have a s32k146 based project on s32ds for ARM v2.2 with no external SDK attached.
I want to migrate this project to s32ds for s32 platform v3.5. How would I go about it. I have tried link below. But no luck
In the available migration window, only this shows up "Migrate toolchain Arm 32/64 NXP GCC 6.3/9.2 to NXP GCC 10.2 for bareboard/library project" and obviously the processor expert doesn't migrate to s32 config tool as it only migrated the toolchain.
Any help is appreciated.
Thank You
Hi @VaneB
Thank you for replying.
As per your suggestion, I moved to S32DS V3.4 and when I opened the migration tool the project was not listed. Also I tried manually selecting the migration filter. But no luck, I have attached the screenshot for your reference.
Hi @Roy2
The migration feature works with SDK and Expert Processor based projects. Check if your project has any SDK attached. Go to Project Properties -> SDK.
Also, make sure you have installed S32SDK S32K1XX RTM 4.0.2 (S32 Design Studio 3.4 S32K1xx Service Pack 1 > S32 Design Studio IDE > S32 Design Studio for S32 Platform v.3.4).
Hi @VaneB
Thank you for you response.
I can confirm that the project is based on Processor Expert and I'm using the SDK's functions and data types, but weirdly when I go to Project Properties -> SDK I cannot find any SDK attached.
Currently, In S32DS for ARM 2.2, I have installed S32SDK_S32K1xx_RTM_3.0.0 SDK. Now it is possible that the project was based on an older SDK, if so how can I verify that.
Regards,
Roy2
Hi @Roy2
Since your project appears to not have attached an SDK or a compatible SDK, the migrate feature will not be available for your project.
You can verify if your project has attached an older SDK in the project Properties -> Processor Expert -> S32 SDK Specific.