How to get .Elf tat has been built under binaries in project explorer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get .Elf tat has been built under binaries in project explorer

1,420 次查看
vignesh_v
Contributor III

I'm using nxp s32 for power architecture 2017_R1. I tried  to create  a project out of single in toggle mpc5777c elf example and build it.

When i built it says the elf. File has been created in the console and but in the project explorer window the binaries is not getting displayed

Under my project name above includes

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,323 次查看
vignesh_v
Contributor III

Yes I had to change refresh policy then it worked thanks

0 项奖励
回复

1,323 次查看
stanish
NXP Employee
NXP Employee

Hi Vignesh,

If the elf file has been created = successfully built (you can check it in the build console)

pastedImage_2.png

then this is perhaps IDE refresh issue. Please try to refresh IDE by hitting F5 or go menu "File->Refresh"

and you should be able to see the elf file under binaries:

pastedImage_4.png

hope it helps.

Stan

0 项奖励
回复