How to build BSP/PSP/library in S32DS IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build BSP/PSP/library in S32DS IDE

5,678 次查看
jianlongzhang
NXP Employee
NXP Employee

Dear All,

 

I downloaded MQX 4.2 for Halo Rev 6 package and wanted to run examples in S32DS. Unfortunately, there is few description about how to build BSP/PSP library in S32DS only below information.

 

pastedImage_1.png

Firstly, I import project '\MQX_4_2_Halo_0_6\mqx\build\s32ds\bsp_mac57d5mb\bsp_mac57d5mb_A5' to S32DS, but failed to build, error shown below.

pastedImage_6.png

 

Could anyone help me build BSP and PSP in S32DS, thank you very much!

 

Best Regards

Tony Zhang

标记 (3)
0 项奖励
回复
7 回复数

5,336 次查看
almarto
Contributor IV

Hi Tony,

You're welcome! We are still trying to troubleshoot this error but we have not succeeded yet, please let me know if you get any result since this is really important for us and our project development. We have not able to execute any project involving DCU in deliverable MQX_4_2_Halo_0_6.rar with S32DS v1.3.

Could anybody at NXP provide some feedback or guide on how to do it?

Thank you very much for you kind collaboration.

Best regards,

alvaro

0 项奖励
回复

5,333 次查看
almarto
Contributor IV

Here is the attached documents. Hope this helps to build "hello" example.

BR

0 项奖励
回复

5,333 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi Alvaro,

Many thanks for your sharing. I can run "Hello" now!

BTW, do you figure out problems of "Tiger" project? I followed your guide, active BSPCFG_ENABLE_DCU, but it cannot display. 

Best Regards

Tony

0 项奖励
回复

5,333 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Tony,

the reason why ovg examples can't be build is missing post-build step in bsp/psp project. Here is step by step guide for fixing the build issue for Logo/tiger and other examples:

  • build bsp/psp for both cores (A5, M4)
  •  start windows command line 
  • go to your MQX_4_2_Halo_0_6 install path (for me it is C:\Freescale\MQX_4_2_Halo_0_6)
  • go to mxq/build/bat sub folder - in sequence start all 4 bat files with 3 arguments. 

          arg 1. MQX_ROOT_DIR (in my case  C:\Freescale\MQX_4_2_Halo_0_6)       

          arg 2. OUTPUT_PATH (in my case  C:\Freescale\MQX_4_2_Halo_0_6\lib\mac57d5mb_a5.s32ds\debug\bsp

          arg 3. s32ds  (tool name)

I used for all 4 .bat files output path with bsp at the end - even when the bat file is related to psp. You have to only change core in the output path related to .bat file (a5 or m4). 

Here are exact command lines how  I used them on my machine: 
bsp_mac57d5mb_m4.bat C:\Freescale\MQX_4_2_Halo_0_6 C:\Freescale\MQX_4_2_Halo_0_6\lib\mac57d5mb_m4.s32ds\debug\bsp s32ds
psp_mac57d5mb_m4.bat C:\Freescale\MQX_4_2_Halo_0_6 C:\Freescale\MQX_4_2_Halo_0_6\lib\mac57d5mb_m4.s32ds\debug\bsp s32ds
bsp_mac57d5mb_a5.bat C:\Freescale\MQX_4_2_Halo_0_6 C:\Freescale\MQX_4_2_Halo_0_6\lib\mac57d5mb_a5.s32ds\debug\bsp s32ds
psp_mac57d5mb_a5.bat C:\Freescale\MQX_4_2_Halo_0_6 C:\Freescale\MQX_4_2_Halo_0_6\lib\mac57d5mb_a5.s32ds\debug\bsp s32ds

Hope it helps. 

Jiri

0 项奖励
回复

5,333 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi Jiri,

Many thanks for your reply!

Would you please share .bat file you mentioned? I will try on my side. Thanks a lot.

Best Regards

Tony

0 项奖励
回复

5,333 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Tony, 

.bat files are part of MQX installation. They are located at [YOUR_MQX_HALO_INSTALL_PATH]/mqx/build/bat as mentioned in point 4. You only need to pass correct arguments.

Jiri

0 项奖励
回复

5,333 次查看
almarto
Contributor IV

Hi Tony,

We also found the same problem and solved it by modifying paths. We were able to build hello example but have found many issues when trying to build tiger example (activating DCU).

Find attached an explanatory document that we have forwarded to NXP waiting for feedback.

BR

0 项奖励
回复