How do I use Jlink to enter attach mode and debug the S32K144?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use Jlink to enter attach mode and debug the S32K144?

2,531 Views
jason_zhong0224
Contributor I

Dears:

OS: Win10

IDE:  S32 Design Studio for ARM Version 2018.R1

Board: S32K144 chip

Debugger: P&E Multilink Universal &J-Link

Problem:Recently I had a problem debugging the S32K144 with jlink and could not get into attach mode !But I can enter attach mode normally using P&E.

Requirements: Could you please tell me how to use jlink to enter attach mode?

   Thank you~

Best regards!

0 Kudos
Reply
5 Replies

2,478 Views
jason_zhong0224
Contributor I

Can someone help me

0 Kudos
Reply

2,475 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it is similar like PE Micro attach. Here is j-ling configuration for attaching to running target: 

jiri_kral_0-1668094483481.png

 

With older Segger j-link driver even with attach was performed Reset. If you met this issue - download new driver from Segger's web page. Installer will ask if S32DS should be updated as well. 

 

Hope it helps. 

 

Jiri

0 Kudos
Reply

2,473 Views
jason_zhong0224
Contributor I

jason_zhong0224_0-1668095312739.png

Hi,jiri:

       I have tried using jlink to get into attach mode, but my S32 design prompts that attach mode is not supported for now. I also follow the method of using jlink to attach mode on the Internet. The procedure is similar to your screenshot. But you can't get in, I'm using PE so it's easy to get into attach mode.

So I was wondering have you successfully used jlink to get into attach mode?

0 Kudos
Reply

2,465 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, I'm able attach the running target. Try to update j-link driver. 

0 Kudos
Reply

2,463 Views
jason_zhong0224
Contributor I
What version of your jlink driver is?
0 Kudos
Reply