How do I use Jlink to enter attach mode and debug the S32K144?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I use Jlink to enter attach mode and debug the S32K144?

2,767 次查看
jason_zhong0224
Contributor I

Dears:

OS: Win10

IDE:  S32 Design Studio for ARM Version 2018.R1

Board: S32K144 chip

Debugger: P&E Multilink Universal &J-Link

Problem:Recently I had a problem debugging the S32K144 with jlink and could not get into attach mode !But I can enter attach mode normally using P&E.

Requirements: Could you please tell me how to use jlink to enter attach mode?

   Thank you~

Best regards!

0 项奖励
回复
5 回复数

2,714 次查看
jason_zhong0224
Contributor I

Can someone help me

0 项奖励
回复

2,711 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it is similar like PE Micro attach. Here is j-ling configuration for attaching to running target: 

jiri_kral_0-1668094483481.png

 

With older Segger j-link driver even with attach was performed Reset. If you met this issue - download new driver from Segger's web page. Installer will ask if S32DS should be updated as well. 

 

Hope it helps. 

 

Jiri

0 项奖励
回复

2,709 次查看
jason_zhong0224
Contributor I

jason_zhong0224_0-1668095312739.png

Hi,jiri:

       I have tried using jlink to get into attach mode, but my S32 design prompts that attach mode is not supported for now. I also follow the method of using jlink to attach mode on the Internet. The procedure is similar to your screenshot. But you can't get in, I'm using PE so it's easy to get into attach mode.

So I was wondering have you successfully used jlink to get into attach mode?

0 项奖励
回复

2,701 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, I'm able attach the running target. Try to update j-link driver. 

0 项奖励
回复

2,699 次查看
jason_zhong0224
Contributor I
What version of your jlink driver is?
0 项奖励
回复