How can I use the S32V234 Vision SDK1.1.1 together with the S32v234 GPU driver module galcore.ko?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I use the S32V234 Vision SDK1.1.1 together with the S32v234 GPU driver module galcore.ko?

跳至解决方案
6,265 次查看
zhangweikanghus
Contributor III

Hi,expert

    I have a s32v234evb28899 borad in my commpany, and I found that I could use Linux BSP17.0 with the VSDK1.1.1。I used the uboot and linux Image created by the Linux BSP17.0(add patch from VSDK1.1.1)  as uboot and lmage. And I used the dtb and rootfs.tar.gz from VSDK1.1.1 's build_content 'v234_linux_build'. It worked well and I could use the demo elf from the vsdk.

   Unfortunately, I followed the user manual of Auto BSP17.0 to add GPU drivers. It caused that the VSDK drived modules failed to insmod. I just changed the menuconfig and setted CMA size to 32MB as below.

pastedImage_1.png

     Then the error log was:

U-Boot 2016.01+g61ddb5d (May 28 2018 - 11:51:10 +0700)

CPU:   NXP S32V234 V1.0 at 800 MHz

Reset cause: External reset

Board: s32v234evb28899

I2C:   ready

DRAM:  256 MiB

All (4) cores are up.

MMC:   FSL_SDHC: 0

Setting PCIE Vendor and Device ID

Forcing PCIe to Gen1 operation

phy link never came up

DEBUG_R0: 0x0044e700, DEBUG_R1: 0x08200000

In:    serial

Out:   serial

Err:   serial

The security module (CSE3) is disabled.

Net:   

Warning: System is using default MAC address. Please set a new value

FEC

Hit any key to stop autoboot:  0 

=> run nfsboot

Booting from net using tftp and nfs...

Using FEC device

TFTP from server 192.168.1.30; our IP address is 192.168.1.35

Filename 'Image'.

Load address: 0x8007ffc0

Loading: #################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

#################################################################

###################

509.8 KiB/s

done

Bytes transferred = 7900016 (788b70 hex)

Using FEC device

TFTP from server 192.168.1.30; our IP address is 192.168.1.35

Filename 's32v234-evb28899.dtb'.

Load address: 0x82000000

Loading: ##

301.8 KiB/s

done

Bytes transferred = 21698 (54c2 hex)

## Flattened Device Tree blob at 82000000

   Booting using the fdt blob at 0x82000000

   reserving fdt memory region: addr=80000000 size=10000

   Loading Device Tree to 000000008fd64000, end 000000008fd6c4c1 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Initializing cgroup subsys cpu

[    0.000000] Linux version 4.1.26-rt29-dirty (root@ubuntu) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9) ) #3 SMP PREEMPT Tue Aug 21 17:50:05 CST 2018

[    0.000000] CPU: AArch64 Processor [410fd034] revision 4

[    0.000000] Detected VIPT I-cache on CPU0

[    0.000000] alternatives: enabling workaround for ARM erratum 845719

[    0.000000] cma: Reserved 32 MiB at 0x00000000c9000000

[    0.000000] PERCPU: Embedded 16 pages/cpu @ffffffc048f96000 s27352 r8192 d29992 u65536

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 85345

[    0.000000] Kernel command line: console=ttyLF0,115200 root=/dev/nfs rw ip=192.168.1.35:192.168.1.30::255.255.255.0::eth0:off nfsroot=192.168.1.30:/tftpboot/rfs,nolock

[    0.000000] PID hash table entries: 2048 (order: 2, 16384 bytes)

[    0.000000] Dentry cache hash table entries: 65536 (order: 7, 524288 bytes)

[    0.000000] Inode-cache hash table entries: 32768 (order: 6, 262144 bytes)

[    0.000000] software IO TLB [mem 0x86ffd000-0x8affd000] (64MB) mapped at [ffffffc006ffd000-ffffffc00affcfff]

[    0.000000] Memory: 209396K/346112K available (5308K kernel code, 310K rwdata, 1828K rodata, 244K init, 270K bss, 103948K reserved, 32768K cma-reserved)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vmalloc : 0xffffff8000000000 - 0xffffffbdffff0000   (   247 GB)

[    0.000000]     vmemmap : 0xffffffbe00000000 - 0xffffffbfc0000000   (     7 GB maximum)

[    0.000000]               0xffffffbe00000000 - 0xffffffbe01068000   (    16 MB actual)

[    0.000000]     fixed   : 0xffffffbffabfd000 - 0xffffffbffac00000   (    12 KB)

[    0.000000]     PCI I/O : 0xffffffbffae00000 - 0xffffffbffbe00000   (    16 MB)

[    0.000000]     modules : 0xffffffbffc000000 - 0xffffffc000000000   (    64 MB)

[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc04b000000   (  1200 MB)

[    0.000000]       .init : 0xffffffc000779000 - 0xffffffc0007b6000   (   244 KB)

[    0.000000]       .text : 0xffffffc000080000 - 0xffffffc000778984   (  7139 KB)

[    0.000000]       .data : 0xffffffc0007bb000 - 0xffffffc000808b70   (   311 KB)

[    0.000000] Preemptible hierarchical RCU implementation.

[    0.000000] RCU dyntick-idle grace-period acceleration is enabled.

[    0.000000] Additional per-CPU info printed with stalls.

[    0.000000] NR_IRQS:64 nr_irqs:64 0

[    0.000000] Architected cp15 timer(s) running at 12.00MHz (virt).

[    0.000000] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2c47f4ee7, max_idle_ns: 440795202497 ns

[    0.000005] sched_clock: 56 bits at 12MHz, resolution 83ns, wraps every 4398046511096ns

[    0.000394] Console: colour dummy device 80x25

[    0.000408] Calibrating delay loop (skipped), value calculated using timer frequency.. 24.00 BogoMIPS (lpj=120000)

[    0.000419] pid_max: default: 32768 minimum: 301

[    0.000513] Security Framework initialized

[    0.000571] Mount-cache hash table entries: 1024 (order: 1, 8192 bytes)

[    0.000580] Mountpoint-cache hash table entries: 1024 (order: 1, 8192 bytes)

[    0.001263] hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available

[    0.080272] CPU1: Booted secondary processor

[    0.080279] Detected VIPT I-cache on CPU1

[    0.100249] CPU2: Booted secondary processor

[    0.100257] Detected VIPT I-cache on CPU2

[    0.120251] CPU3: Booted secondary processor

[    0.120255] Detected VIPT I-cache on CPU3

[    0.120335] Brought up 4 CPUs

[    0.120361] SMP: Total of 4 processors activated.

[    0.120366] CPU: All CPU(s) started at EL1

[    0.120397] alternatives: patching kernel code

[    0.120925] devtmpfs: initialized

[    0.125207] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

[    0.126655] pinctrl core: initialized pinctrl subsystem

[    0.127430] NET: Registered protocol family 16

[    0.150083] cpuidle: using governor ladder

[    0.190372] cpuidle: using governor menu

[    0.190465] vdso: 2 pages (1 code @ ffffffc0007c1000, 1 data @ ffffffc0007c0000)

[    0.190511] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.

[    0.191857] DMA: preallocated 256 KiB pool for atomic allocations

[    0.207077] ACPI: Interpreter disabled.

[    0.210433] vgaarb: loaded

[    0.210729] SCSI subsystem initialized

[    0.211024] usbcore: registered new interface driver usbfs

[    0.211084] usbcore: registered new interface driver hub

[    0.211170] usbcore: registered new device driver usb

[    0.211441] imx-i2c 40051000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c0grp, deferring probe

[    0.211561] imx-i2c 400b8000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c1grp, deferring probe

[    0.211588] imx-i2c 400ba000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c2grp, deferring probe

[    0.211714] pps_core: LinuxPPS API ver. 1 registered

[    0.211721] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

[    0.211751] PTP clock support registered

[    0.212685] Switched to clocksource arch_sys_counter

[    0.213181] pnp: PnP ACPI: disabled

[    0.221423] NET: Registered protocol family 2

[    0.221949] TCP established hash table entries: 4096 (order: 3, 32768 bytes)

[    0.222003] TCP bind hash table entries: 4096 (order: 4, 65536 bytes)

[    0.222089] TCP: Hash tables configured (established 4096 bind 4096)

[    0.222148] UDP hash table entries: 256 (order: 1, 8192 bytes)

[    0.222171] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

[    0.222371] NET: Registered protocol family 1

[    0.222649] RPC: Registered named UNIX socket transport module.

[    0.222656] RPC: Registered udp transport module.

[    0.222662] RPC: Registered tcp transport module.

[    0.222667] RPC: Registered tcp NFSv4.1 backchannel transport module.

[    0.224153] futex hash table entries: 1024 (order: 4, 65536 bytes)

[    0.224791] HugeTLB registered 2 MB page size, pre-allocated 0 pages

[    0.226193] fuse init (API version 7.23)

[    0.227088] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 249)

[    0.227105] io scheduler noop registered

[    0.227115] io scheduler deadline registered

[    0.227155] io scheduler cfq registered (default)

[    0.227609] s32v234-siul2-pinctrl 4006c240.siul2-pinctrl: initialized s32 pinctrl driver

[    0.230597] fsl_dcu 40028000.dcu: DCU: surface memory space is [0xC0000000, 0xC1000000].

[    0.231300] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb0> : <1920 x 1080>

[    0.231595] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb1> : <1920 x 1080>

[    0.231876] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb2> : <1920 x 1080>

[    0.232152] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb3> : <1920 x 1080>

[    0.232436] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb4> : <1920 x 1080>

[    0.232747] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb5> : <1920 x 1080>

[    0.233167] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb6> : <1920 x 1080>

[    0.233463] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb7> : <1920 x 1080>

[    0.234327] 40053000.serial: ttyLF0 at MMIO 0x40053000 (irq = 24, base_baud = 4166666) is a FSL_LINFLEX

[    0.898964] console [ttyLF0] enabled

[    0.903128] 400bc000.serial: ttyLF1 at MMIO 0x400bc000 (irq = 43, base_baud = 4166666) is a FSL_LINFLEX

[    0.913166] Unable to detect cache hierarcy from DT for CPU 0

[    0.922987] loop: module loaded

[    0.929309] libphy: Fixed MDIO Bus: probed

[    0.933940] tun: Universal TUN/TAP device driver, 1.6

[    0.939028] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>

[    0.945455] vcan: Virtual CAN interface driver

[    0.949936] slcan: serial line CAN interface driver

[    0.954936] slcan: 10 dynamic interface channels.

[    0.959680] CAN device driver interface

[    0.964409] flexcan 40055000.flexcan: device registered (reg_base=ffffff800007a000, irq=25)

[    0.973624] flexcan 400be000.flexcan: device registered (reg_base=ffffff800007c000, irq=44)

[    0.982728] pps pps0: new PPS source ptp0

[    0.988455] libphy: fec_enet_mii_bus: probed

[    0.993906] fec 40032000.ethernet eth0: registered PHC device 0

[    1.000375] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

[    1.007016] ehci-pci: EHCI PCI platform driver

[    1.011543] ehci-platform: EHCI generic platform driver

[    1.017082] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver

[    1.023353] ohci-pci: OHCI PCI platform driver

[    1.027889] ohci-platform: OHCI generic platform driver

[    1.033652] usbcore: registered new interface driver usb-storage

[    1.040032] i2c /dev entries driver

[    1.044348] sac58r-wdt 4000a000.swt: SAC58R/S32V234 Watchdog Timer Registered. timeout=30s (nowayout=0)

[    1.054019] sdhci: Secure Digital Host Controller Interface driver

[    1.060244] sdhci: Copyright(c) Pierre Ossman

[    1.064657] sdhci-pltfm: SDHCI platform and OF driver helper

[    1.071152] /soc/aips-bus@40000000/usdhc@4005D000: voltage-ranges unspecified

[    1.078581] sdhci-esdhc-imx 4005d000.usdhc: No vmmc regulator found

[    1.084917] sdhci-esdhc-imx 4005d000.usdhc: No vqmmc regulator found

[    1.132721] mmc0: SDHCI controller on 4005d000.usdhc [4005d000.usdhc] using ADMA

[    1.140602] usbcore: registered new interface driver usbhid

[    1.146237] usbhid: USB HID core driver

[    1.164936] NET: Registered protocol family 10

[    1.170121] sit: IPv6 over IPv4 tunneling driver

[    1.175377] NET: Registered protocol family 17

[    1.179870] can: controller area network core (rev 20120528 abi 9)

[    1.186176] NET: Registered protocol family 29

[    1.190690] can: raw protocol (rev 20120528)

[    1.195021] can: broadcast manager protocol (rev 20120528 t)

[    1.200732] can: netlink gateway (rev 20130117) max_hops=1

[    1.206338] Key type dns_resolver registered

[    1.207553] mmc0: MAN_BKOPS_EN bit is not set

[    1.215592] mmc0: new DDR MMC card at address 0001

[    1.215705] registered taskstats version 1

[    1.216508] i2c i2c-0: IMX I2C adapter registered

[    1.216536] i2c i2c-0: using dma0chan2 (tx) and dma0chan3 (rx) for DMA transfers

[    1.237147] mmcblk0: mmc0:0001 MMC32G 29.0 GiB 

[    1.241807] mmcblk0boot0: mmc0:0001 MMC32G partition 1 16.0 MiB

[    1.247952] mmcblk0boot1: mmc0:0001 MMC32G partition 2 16.0 MiB

[    1.254032] mmcblk0rpmb: mmc0:0001 MMC32G partition 3 128 KiB

[    1.260598]  mmcblk0: p1 p2

[    1.262738] Sii902x: read id = 0xB0-0x02-0x03-0x00

[    1.303681] i2c i2c-1: IMX I2C adapter registered

[    1.308462] i2c i2c-1: using dma0chan18 (tx) and dma0chan19 (rx) for DMA transfers

[    1.316680] i2c i2c-2: IMX I2C adapter registered

[    1.321446] i2c i2c-2: using dma0chan20 (tx) and dma0chan21 (rx) for DMA transfers

[    1.329135] hctosys: unable to open rtc device (rtc0)

[    1.412799] fec 40032000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=40032000.etherne:07, irq=-1)

[    1.425998] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

[    5.413383] fec 40032000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx

[    5.422715] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

[    5.442833] IP-Config: Complete:

[    5.446090]      device=eth0, hwaddr=00:1b:c3:12:34:22, ipaddr=192.168.1.35, mask=255.255.255.0, gw=255.255.255.255

[    5.456639]      host=192.168.1.35, domain=, nis-domain=(none)

[    5.462515]      bootserver=192.168.1.30, rootserver=192.168.1.30, rootpath=

[    5.661373] VFS: Mounted root (nfs filesystem) on device 0:15.

[    5.681579] devtmpfs: mounted

[    5.684382] Freeing unused kernel memory: 244K (ffffffc000779000 - ffffffc0007b6000)

[    5.691897] Freeing alternatives memory: 12K (ffffffc0007b6000 - ffffffc0007b9000)

INIT: version 2.88 booting

Starting udev

[    7.928417] udevd[634]: starting version 3.2.2

[    8.063109] random: udevd urandom read with 25 bits of entropy available

[    8.482798] udevd[635]: starting eudev-3.2.2

Tue Mar  6 12:40:16 UTC 2018

INIT: Entering runlevel: 5

Configuring network interfaces... RTNETLINK answers: File exists

ifup skipped for nfsroot interface eth0

run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1

Starting OpenBSD Secure Shell server: sshd

done.

Starting rpcbind daemon...done.

starting statd: done

Starting network benchmark server: netserver.

exportfs: can't open /etc/exports for reading

NFS daemon support not enabled in kernel

Starting syslogd/klogd: done

Starting internet superserver: xinetd.

[   16.007162] loading NXP PHY driver: [autonomous mode]

Auto Linux BSP 1.0 s32v234evb /dev/ttyLF0

s32v234evb login: [   55.412757] random: nonblocking pool is initialized

Auto Linux BSP 1.0 s32v234evb /dev/ttyLF0

s32v234evb login: root

root@s32v234evb:~# cd /s32v234/

root@s32v234evb:/s32v234# ls

apex.ko  cam.ko  csi.ko  fdma.ko  galcore.ko  h264dcd.ko  h264enc.ko  jpegdcd.ko  oal_cma.ko  seq.ko  sm_drv.ko  viulite.ko

root@s32v234evb:/s32v234# insmod apex.ko 

[  250.228863] Unable to handle kernel NULL pointer dereference at virtual address 00000003

[  250.236627] pgd = ffffffc046397000

[  250.239958] [00000003] *pgd=00000000c5ce2003, *pud=00000000c5ce2003, *pmd=0000000000000000

[  250.248185] Internal error: Oops: 96000006 [#1] PREEMPT SMP

[  250.253719] Modules linked in: apex(O+) nxp sja1105pqrs(O)

[  250.259176] CPU: 1 PID: 881 Comm: insmod Tainted: G           O    4.1.26-rt29-dirty #3

[  250.267132] Hardware name: Freescale S32V234 (DT)

[  250.271808] task: ffffffc0462be3c0 ti: ffffffc045a60000 task.ti: ffffffc045a60000

[  250.279260] PC is at apex_probe+0x24/0x280 [apex]

[  250.283928] LR is at apex_probe+0x24/0x280 [apex]

[  250.288596] pc : [<ffffffbffc0382dc>] lr : [<ffffffbffc0382dc>] pstate: 20000145

[  250.295950] sp : ffffffc045a63ac0

[  250.299239] x29: ffffffc045a63ac0 x28: 0000000000000124 

[  250.304517] x27: ffffffc045b8fc00 x26: ffffffc0000f91d0 

[  250.309796] x25: ffffffc0464ac5c0 x24: ffffffbffc038bf0 

[  250.315075] x23: 0000000000000006 x22: ffffffc04623d400 

[  250.320354] x21: ffffffbffc038b18 x20: ffffffbffc038af0 

[  250.325633] x19: ffffffc04623d410 x18: 0000000000000000 

[  250.330912] x17: ffffffc000611200 x16: 0000000000000000 

[  250.336190] x15: 0000000000000001 x14: ffffffc0451a890a 

[  250.341469] x13: ffffffc0451a8909 x12: 0000000000000030 

[  250.346749] x11: 0000000000000004 x10: 0101010101010101 

[  250.352028] x9 : fffffffffffffff9 x8 : 7f7f7f7f7f7f7f7f 

[  250.357308] x7 : fefefeff646c606d x6 : 0f121e0ce7eee5e4 

[  250.362587] x5 : 64656e670c1e120f x4 : 0000000000000000 

[  250.367867] x3 : 0000000000000140 x2 : 00000000000035b2 

[  250.373146] x1 : ffffffc045a60000 x0 : 0000000000000000 

[  250.378424] 

[  250.379899] Process insmod (pid: 881, stack limit = 0xffffffc045a60028)

[  250.386476] Stack: (0xffffffc045a63ac0 to 0xffffffc045a64000)

[  250.392192] 3ac0: 45a63b00 ffffffc0 0039c80c ffffffc0 4623d410 ffffffc0 fc038af0 ffffffbf

[  250.400326] 3ae0: fc038b18 ffffffbf 00832000 ffffffc0 45a63b00 ffffffc0 0039c7f4 ffffffc0

[  250.408460] 3b00: 45a63b30 ffffffc0 0039b044 ffffffc0 4623d410 ffffffc0 00000000 00000000

[  250.416595] 3b20: fc038b18 ffffffbf 00832000 ffffffc0 45a63b70 ffffffc0 0039b27c ffffffc0

[  250.424730] 3b40: 4623d410 ffffffc0 fc038b18 ffffffbf 4623d470 ffffffc0 007e6670 ffffffc0

[  250.432865] 3b60: 007e6000 ffffffc0 003993ac ffffffc0 45a63ba0 ffffffc0 003993a0 ffffffc0

[  250.440999] 3b80: 00000000 00000000 fc038b18 ffffffbf 0039b1e0 ffffffc0 fc038bf0 ffffffbf

[  250.449134] 3ba0: 45a63be0 ffffffc0 0039aa68 ffffffc0 fc038b18 ffffffbf 466957c0 ffffffc0

[  250.457268] 3bc0: 00000000 00000000 0059d690 ffffffc0 0fd202a8 ffffffc0 461ab168 ffffffc0

[  250.465403] 3be0: 45a63bf0 ffffffc0 0039a6d8 ffffffc0 45a63c30 ffffffc0 0039b6a8 ffffffc0

[  250.473538] 3c00: fc038b18 ffffffbf 007c8e20 ffffffc0 451a8180 ffffffc0 fc03b000 ffffffbf

[  250.481672] 3c20: 00000000 00000000 45a63c70 ffffffc0 45a63c50 ffffffc0 0039c73c ffffffc0

[  250.489806] 3c40: 007c8e20 ffffffc0 007c8e20 ffffffc0 45a63c60 ffffffc0 fc03b018 ffffffbf

[  250.497941] 3c60: 45a63c70 ffffffc0 00081024 ffffffc0 45a63cf0 ffffffc0 005a05f4 ffffffc0

[  250.506076] 3c80: fc038ba0 ffffffbf 007d0000 ffffffc0 464ac5d0 ffffffc0 45eecd80 ffffffc0

[  250.514210] 3ca0: fc038ba0 ffffffbf 45eecd80 ffffffc0 00000001 00000000 00000001 00000000

[  250.522346] 3cc0: 45a63cf0 ffffffc0 005a05c0 ffffffc0 fc038ba0 ffffffbf 007d0000 ffffffc0

[  250.530480] 3ce0: 464ac5d0 ffffffc0 00000001 00000000 45a63d20 ffffffc0 000fc1c4 ffffffc0

[  250.538615] 3d00: 45a63e68 ffffffc0 00000001 00000000 464ac5d0 ffffffc0 00000001 00000000

[  250.546749] 3d20: 45a63e30 ffffffc0 000fc8b8 ffffffc0 00000000 00000000 00000003 00000000

[  250.554883] 3d40: 00419550 00000000 9485b9c4 0000007f 80000000 00000000 00000015 00000000

[  250.563018] 3d60: 0000011a 00000000 00000111 00000000 005ac000 ffffffc0 45a60000 ffffffc0

[  250.571153] 3d80: 45a63e30 ffffffc0 45a63de8 ffffffc0 006e8280 ffffffc0 00000003 0000006e

[  250.579287] 3da0: 0000003f ffffffbf 0000feff ffffff80 0000fff1 ffffff80 005b5368 ffffffc0

[  250.587422] 3dc0: fc03b048 ffffffbf 45a63e28 ffffffc0 0000000f 000081a4 00000001 000003e8

[  250.595556] 3de0: 000003e8 00000000 0004d118 00000000 5b7b88ba 00000000 00000000 00000000

[  250.603690] 3e00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[  250.611825] 3e20: 00000000 00000000 00000000 00000000 e5a2cc30 0000007f 00084470 ffffffc0

[  250.619960] 3e40: 00000000 00000000 1bcba780 00000000 ffffffff ffffffff 00000000 00000000

[  250.628095] 3e60: 45a63ec0 ffffffc0 01312000 ffffff80 0004d118 00000000 0135e818 ffffff80

[  250.636230] 3e80: 0135e6c8 ffffff80 0133b2c8 ffffff80 00000e58 00000000 00001230 00000000

[  250.644364] 3ea0: 00000000 00000000 00000000 00000000 00001050 00000000 00000022 00000023

[  250.652499] 3ec0: 0000000e 00000000 0000000a 00000000 00000003 00000000 00419550 00000000

[  250.660633] 3ee0: 00000000 00000000 00000003 00000000 00000000 00000000 ffffffff 60ceffff

[  250.668768] 3f00: ffffffff ffffffff ffffffff ffffffff 00000111 00000000 00000005 00000000

[  250.676902] 3f20: 01010101 01010101 00000001 00000000 00000000 00000000 00000000 00000000

[  250.685038] 3f40: 94928700 0000007f 0000073f 00000000 9485b9a0 0000007f 0042a618 00000000

[  250.693173] 3f60: 00000000 00000000 00419550 00000000 1bcba780 00000000 00000000 00000000

[  250.701307] 3f80: 00000000 00000000 00000000 00000000 00000000 00000000 00000002 00000000

[  250.709442] 3fa0: 00000000 00000000 00000000 00000000 00000000 00000000 e5a2cc30 0000007f

[  250.717577] 3fc0: 004108c4 00000000 e5a2cc30 0000007f 9485b9c4 0000007f 80000000 00000000

[  250.725712] 3fe0: 00000003 00000000 00000111 00000000 00000000 00000000 00000000 00000000

[  250.733840] Call trace:

[  250.736273] [<ffffffbffc0382dc>] apex_probe+0x24/0x280 [apex]

[  250.741984] [<ffffffc00039c80c>] platform_drv_probe+0x4c/0xb8

[  250.747692] [<ffffffc00039b044>] driver_probe_device+0x16c/0x2b0

[  250.753660] [<ffffffc00039b27c>] __driver_attach+0x9c/0xa0

[  250.759112] [<ffffffc0003993a0>] bus_for_each_dev+0x60/0xa0

[  250.764650] [<ffffffc00039aa68>] driver_attach+0x20/0x28

[  250.769928] [<ffffffc00039a6d8>] bus_add_driver+0x150/0x208

[  250.775467] [<ffffffc00039b6a8>] driver_register+0x60/0x120

[  250.781006] [<ffffffc00039c73c>] __platform_driver_register+0x5c/0x68

[  250.787414] [<ffffffbffc03b018>] ApexInit+0x18/0x48 [apex]

[  250.792864] [<ffffffc000081024>] do_one_initcall+0x8c/0x1a8

[  250.798401] [<ffffffc0005a05f4>] do_init_module+0x5c/0x1a4

[  250.803854] [<ffffffc0000fc1c4>] load_module+0x17f4/0x1c88

[  250.809304] [<ffffffc0000fc8b8>] SyS_finit_module+0xc8/0xd8

[  250.814843] Code: 9100f3a2 58001041 f940fc00 9510dcd0 (39c00c15) 

[  250.820984] ---[ end trace fee402510e2c9983 ]---

Segmentation fault

root@s32v234evb:/s32v234# 

In addition, if I didn't set the CMA size, the right log was as below:

U-Boot 2016.01+g61ddb5d (May 28 2018 - 11:51:10 +0700)

CPU: NXP S32V234 V1.0 at 800 MHz
Reset cause: External reset
Board: s32v234evb28899
I2C: ready
DRAM: 256 MiB
All (4) cores are up.
MMC: FSL_SDHC: 0
Setting PCIE Vendor and Device ID

Forcing PCIe to Gen1 operation
phy link never came up
DEBUG_R0: 0x0071d600, DEBUG_R1: 0x08200000
In: serial
Out: serial
Err: serial
The security module (CSE3) is disabled.
Net:
Warning: System is using default MAC address. Please set a new value
FEC
Hit any key to stop autoboot: 0
=> run nfsboot
Booting from net using tftp and nfs...
Using FEC device
TFTP from server 192.168.1.30; our IP address is 192.168.1.35
Filename 'Image'.
Load address: 0x8007ffc0
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
##############
531.3 KiB/s
done
Bytes transferred = 7833088 (778600 hex)
Using FEC device
TFTP from server 192.168.1.30; our IP address is 192.168.1.35
Filename 's32v234-evb28899.dtb'.
Load address: 0x82000000
Loading: ##
470.7 KiB/s
done
Bytes transferred = 21698 (54c2 hex)
## Flattened Device Tree blob at 82000000
Booting using the fdt blob at 0x82000000
reserving fdt memory region: addr=80000000 size=10000
Loading Device Tree to 000000008fd64000, end 000000008fd6c4c1 ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 4.1.26-rt29-dirty (b46809@ulm) (gcc version 6.3.1 20170404 (Linaro GCC 6.3-2017.05) ) #1 SMP PREEMPT Tue Jun 5 21:02:32 CEST 2018
[ 0.000000] CPU: AArch64 Processor [410fd034] revision 4
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] alternatives: enabling workaround for ARM erratum 845719
[ 0.000000] PERCPU: Embedded 16 pages/cpu @ffffffc04af96000 s27288 r8192 d30056 u65536
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 85345
[ 0.000000] Kernel command line: console=ttyLF0,115200 root=/dev/nfs rw ip=192.168.1.35:192.168.1.30::255.255.255.0::eth0:off nfsroot=192.168.1.30:/tftpboot/rfs,nolock
[ 0.000000] PID hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 6, 262144 bytes)
[ 0.000000] software IO TLB [mem 0xc5000000-0xc9000000] (64MB) mapped at [ffffffc045000000-ffffffc048ffffff]
[ 0.000000] Memory: 242228K/346112K available (5260K kernel code, 317K rwdata, 1812K rodata, 240K init, 272K bss, 103884K reserved, 0K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vmalloc : 0xffffff8000000000 - 0xffffffbdffff0000 ( 247 GB)
[ 0.000000] vmemmap : 0xffffffbe00000000 - 0xffffffbfc0000000 ( 7 GB maximum)
[ 0.000000] 0xffffffbe00000000 - 0xffffffbe01068000 ( 16 MB actual)
[ 0.000000] fixed : 0xffffffbffabfd000 - 0xffffffbffac00000 ( 12 KB)
[ 0.000000] PCI I/O : 0xffffffbffae00000 - 0xffffffbffbe00000 ( 16 MB)
[ 0.000000] modules : 0xffffffbffc000000 - 0xffffffc000000000 ( 64 MB)
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc04b000000 ( 1200 MB)
[ 0.000000] .init : 0xffffffc000769000 - 0xffffffc0007a5000 ( 240 KB)
[ 0.000000] .text : 0xffffffc000080000 - 0xffffffc000768874 ( 7075 KB)
[ 0.000000] .data : 0xffffffc0007a9000 - 0xffffffc0007f8600 ( 318 KB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU dyntick-idle grace-period acceleration is enabled.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] Architected cp15 timer(s) running at 12.00MHz (virt).
[ 0.000000] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2c47f4ee7, max_idle_ns: 440795202497 ns
[ 0.000005] sched_clock: 56 bits at 12MHz, resolution 83ns, wraps every 4398046511096ns
[ 0.000388] Console: colour dummy device 80x25
[ 0.000402] Calibrating delay loop (skipped), value calculated using timer frequency.. 24.00 BogoMIPS (lpj=120000)
[ 0.000413] pid_max: default: 32768 minimum: 301
[ 0.000507] Security Framework initialized
[ 0.000564] Mount-cache hash table entries: 1024 (order: 1, 8192 bytes)
[ 0.000572] Mountpoint-cache hash table entries: 1024 (order: 1, 8192 bytes)
[ 0.001252] hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available
[ 0.080274] CPU1: Booted secondary processor
[ 0.080281] Detected VIPT I-cache on CPU1
[ 0.100252] CPU2: Booted secondary processor
[ 0.100260] Detected VIPT I-cache on CPU2
[ 0.120255] CPU3: Booted secondary processor
[ 0.120260] Detected VIPT I-cache on CPU3
[ 0.120340] Brought up 4 CPUs
[ 0.120367] SMP: Total of 4 processors activated.
[ 0.120373] CPU: All CPU(s) started at EL1
[ 0.120404] alternatives: patching kernel code
[ 0.120918] devtmpfs: initialized
[ 0.125090] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.125512] pinctrl core: initialized pinctrl subsystem
[ 0.126256] NET: Registered protocol family 16
[ 0.150087] cpuidle: using governor ladder
[ 0.190374] cpuidle: using governor menu
[ 0.190466] vdso: 2 pages (1 code @ ffffffc0007b1000, 1 data @ ffffffc0007b0000)
[ 0.190514] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.190691] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.205748] ACPI: Interpreter disabled.
[ 0.209010] vgaarb: loaded
[ 0.209288] SCSI subsystem initialized
[ 0.209583] usbcore: registered new interface driver usbfs
[ 0.209639] usbcore: registered new interface driver hub
[ 0.209726] usbcore: registered new device driver usb
[ 0.209952] imx-i2c 40051000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c0grp, deferring probe
[ 0.210062] imx-i2c 400b8000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c1grp, deferring probe
[ 0.210088] imx-i2c 400ba000.i2c: could not find pctldev for node /soc/aips-bus@40000000/siul2/siul2-pinctrl@4006C000/s32v234-evb/i2c2grp, deferring probe
[ 0.210250] pps_core: LinuxPPS API ver. 1 registered
[ 0.210256] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.210289] PTP clock support registered
[ 0.211195] Switched to clocksource arch_sys_counter
[ 0.211710] pnp: PnP ACPI: disabled
[ 0.219128] NET: Registered protocol family 2
[ 0.219714] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.219768] TCP bind hash table entries: 4096 (order: 4, 65536 bytes)
[ 0.219855] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.219916] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 0.219938] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 0.220135] NET: Registered protocol family 1
[ 0.220432] RPC: Registered named UNIX socket transport module.
[ 0.220439] RPC: Registered udp transport module.
[ 0.220444] RPC: Registered tcp transport module.
[ 0.220450] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.222060] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.222671] HugeTLB registered 2 MB page size, pre-allocated 0 pages
[ 0.224031] fuse init (API version 7.23)
[ 0.224873] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 250)
[ 0.224889] io scheduler noop registered
[ 0.224900] io scheduler deadline registered
[ 0.224941] io scheduler cfq registered (default)
[ 0.225393] s32v234-siul2-pinctrl 4006c240.siul2-pinctrl: initialized s32 pinctrl driver
[ 0.228236] fsl_dcu 40028000.dcu: DCU: surface memory space is [0xC0000000, 0xC1000000].
[ 0.228937] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb0> : <1920 x 1080>
[ 0.229218] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb1> : <1920 x 1080>
[ 0.229485] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb2> : <1920 x 1080>
[ 0.229775] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb3> : <1920 x 1080>
[ 0.230048] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb4> : <1920 x 1080>
[ 0.230319] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb5> : <1920 x 1080>
[ 0.230593] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb6> : <1920 x 1080>
[ 0.230865] fsl_dcu 40028000.dcu: Selected video mode on </dev/fb7> : <1920 x 1080>
[ 0.231928] 40053000.serial: ttyLF0 at MMIO 0x40053000 (irq = 24, base_baud = 4166666) is a FSL_LINFLEX
[ 0.954720] console [ttyLF0] enabled
[ 0.959209] 400bc000.serial: ttyLF1 at MMIO 0x400bc000 (irq = 43, base_baud = 4166666) is a FSL_LINFLEX
[ 0.970138] Unable to detect cache hierarcy from DT for CPU 0
[ 0.980390] loop: module loaded
[ 0.986774] libphy: Fixed MDIO Bus: probed
[ 0.991774] tun: Universal TUN/TAP device driver, 1.6
[ 0.997357] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 1.004380] vcan: Virtual CAN interface driver
[ 1.009295] slcan: serial line CAN interface driver
[ 1.014708] slcan: 10 dynamic interface channels.
[ 1.019912] CAN device driver interface
[ 1.024980] flexcan 40055000.flexcan: device registered (reg_base=ffffff800007a000, irq=25)
[ 1.035000] flexcan 400be000.flexcan: device registered (reg_base=ffffff800007c000, irq=44)
[ 1.044886] pps pps0: new PPS source ptp0
[ 1.050194] libphy: fec_enet_mii_bus: probed
[ 1.056003] fec 40032000.ethernet eth0: registered PHC device 0
[ 1.063097] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.070320] ehci-pci: EHCI PCI platform driver
[ 1.075424] ehci-platform: EHCI generic platform driver
[ 1.081429] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.088291] ohci-pci: OHCI PCI platform driver
[ 1.093261] ohci-platform: OHCI generic platform driver
[ 1.099453] usbcore: registered new interface driver usb-storage
[ 1.106407] i2c /dev entries driver
[ 1.110860] sac58r-wdt 4000a000.swt: SAC58R/S32V234 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 1.121440] sdhci: Secure Digital Host Controller Interface driver
[ 1.128272] sdhci: Copyright(c) Pierre Ossman
[ 1.133121] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.140158] /soc/aips-bus@40000000/usdhc@4005D000: voltage-ranges unspecified
[ 1.148132] sdhci-esdhc-imx 4005d000.usdhc: No vmmc regulator found
[ 1.155081] sdhci-esdhc-imx 4005d000.usdhc: No vqmmc regulator found
[ 1.201210] mmc0: SDHCI controller on 4005d000.usdhc [4005d000.usdhc] using ADMA
[ 1.209777] usbcore: registered new interface driver usbhid
[ 1.215969] usbhid: USB HID core driver
[ 1.233500] NET: Registered protocol family 10
[ 1.239102] sit: IPv6 over IPv4 tunneling driver
[ 1.244823] NET: Registered protocol family 17
[ 1.249750] can: controller area network core (rev 20120528 abi 9)
[ 1.256657] NET: Registered protocol family 29
[ 1.261621] can: raw protocol (rev 20120528)
[ 1.266113] mmc0: MAN_BKOPS_EN bit is not set
[ 1.271153] can: broadcast manager protocol (rev 20120528 t)
[ 1.274207] mmc0: new DDR MMC card at address 0001
[ 1.274535] mmcblk0: mmc0:0001 MMC32G 29.0 GiB
[ 1.274625] mmcblk0boot0: mmc0:0001 MMC32G partition 1 16.0 MiB
[ 1.274715] mmcblk0boot1: mmc0:0001 MMC32G partition 2 16.0 MiB
[ 1.274798] mmcblk0rpmb: mmc0:0001 MMC32G partition 3 128 KiB
[ 1.291777] mmcblk0: p1 p2
[ 1.310300] can: netlink gateway (rev 20130117) max_hops=1
[ 1.316472] Key type dns_resolver registered
[ 1.321854] registered taskstats version 1
[ 1.327173] i2c i2c-0: IMX I2C adapter registered
[ 1.332442] i2c i2c-0: using dma0chan2 (tx) and dma0chan3 (rx) for DMA transfers
[ 1.344013] Sii902x: read id = 0xB0-0x02-0x03-0x00
[ 1.392155] i2c i2c-1: IMX I2C adapter registered
[ 1.397391] i2c i2c-1: using dma0chan18 (tx) and dma0chan19 (rx) for DMA transfers
[ 1.406321] i2c i2c-2: IMX I2C adapter registered
[ 1.411580] i2c i2c-2: using dma0chan20 (tx) and dma0chan21 (rx) for DMA transfers
[ 1.501295] fec 40032000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=40032000.etherne:07, irq=-1)
[ 1.515727] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 5.501891] fec 40032000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 5.521218] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 5.541329] IP-Config: Complete:
[ 5.544901] device=eth0, hwaddr=00:1b:c3:12:34:22, ipaddr=192.168.1.35, mask=255.255.255.0, gw=255.255.255.255
[ 5.556480] host=192.168.1.35, domain=, nis-domain=(none)
[ 5.562949] bootserver=192.168.1.30, rootserver=192.168.1.30, rootpath=
[ 5.613165] VFS: Mounted root (nfs filesystem) on device 0:15.
[ 5.623156] devtmpfs: mounted
[ 5.626189] Freeing unused kernel memory: 240K (ffffffc000769000 - ffffffc0007a5000)
[ 5.634530] Freeing alternatives memory: 8K (ffffffc0007a5000 - ffffffc0007a7000)
INIT: version 2.88 booting
Starting udev
[ 7.521473] udevd[629]: starting version 3.2.2
[ 7.606987] random: udevd urandom read with 26 bits of entropy available
[ 7.995568] udevd[630]: starting eudev-3.2.2
Tue Mar 6 12:40:16 UTC 2018
INIT: Entering runlevel: 5
Configuring network interfaces... RTNETLINK answers: File exists
ifup skipped for nfsroot interface eth0
run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1
Starting OpenBSD Secure Shell server: sshd
done.
Starting rpcbind daemon...done.
starting statd: done
Starting network benchmark server: netserver.
exportfs: can't open /etc/exports for reading
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
Starting internet superserver: xinetd.
[ 15.184016] loading NXP PHY driver: [autonomous mode]

Auto Linux BSP 1.0 s32v234evb /dev/ttyLF0

s32v234evb login:
Auto Linux BSP 1.0 s32v234evb /dev/ttyLF0

s32v234evb login: root
root@s32v234evb:~# cd /s32v234/
root@s32v234evb:/s32v234# insmo[ 45.681286] random: nonblocking pool is initialized
root@s32v234evb:/s32v234#
root@s32v234evb:/s32v234#
root@s32v234evb:/s32v234# insmod apex.ko
[ 55.212495] APEX kernel module - IRQ 32, ID 0, 1 devices loaded.
[ 55.218816] APEX kernel module - IRQ 33, ID 1, 2 devices loaded.
root@s32v234evb:/s32v234#

0 项奖励
回复
1 解答
4,941 次查看
nxa13002
NXP Employee
NXP Employee

Did you rebuild VSDK drivers ? . You need to rebuild VSDK drivers after you build Image and dtb

在原帖中查看解决方案

0 项奖励
回复
10 回复数
4,941 次查看
nxa13002
NXP Employee
NXP Employee

Hi ,

I have tried with bsp18_rc7 using following steps:

 

- make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- s32v234_defconfig

- make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- menuconfig

then follow GPU enable instruction above.

Apply Patch from VSDK

- patch -p1 -i $(SDK_ROOT)/os/linux/0001-s32v234-dts-Add-VSDK-specific-configuration.patch

 

Then build vsdk drivers and galcore driver. It can insmod all vsdk drivers and galcore driver

0 项奖励
回复
4,941 次查看
zhangweikanghus
Contributor III

Hi,

Thank you. Can you tell me how can I get bsp18_rc7? I just found bsp17_hf1 in the NXP.com.

0 项奖励
回复
4,941 次查看
nxa13002
NXP Employee
NXP Employee

Hi,

To get bsp_18 rc7 do following steps:

  - Go linux repo

 - git fetch

- git checkout [tag_bsp18]

But I think that you can insmod galcore with bsp17 with the steps:

make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- s32v234_defconfig

- make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- menuconfig

then follow GPU enable instruction above.

Apply Patch from VSDK

- patch -p1 -i $(SDK_ROOT)/os/linux/0001-s32v234-dts-Add-VSDK-specific-configuration.patch

make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu-

And make sure that you have to build again all vsdk drivers and galcore driver

0 项奖励
回复
4,941 次查看
zhangweikanghus
Contributor III

Hi,

   Thank you. Is Your VSDK version  RTM1.2.0 ?

0 项奖励
回复
4,941 次查看
nxa13002
NXP Employee
NXP Employee

Yes, But I am not sure that BSP which is included in VSDK 1.2 that the CMA is enabled or not

0 项奖励
回复
4,941 次查看
zhangweikanghus
Contributor III

Thank you.

You use galcore.ko built by yourself with the VSDK1.2's Image & dtb & rootfs,and it works successfully? 

Does it work successfully with the Image built by BSP18.0?

0 项奖励
回复
4,941 次查看
nxa13002
NXP Employee
NXP Employee

No, I did not use Image and dtb from VSDK1.2 , I built Image and dtb by myself . The Image and dtb from VSDK1.2 did not enable CMA configure .

0 项奖励
回复
4,941 次查看
zhangweikanghus
Contributor III

Can you show your boot log? I built Image in Yocto and enable CMA configure.Then the kernel module in VSDK‘’s rootfs such as apex.ko cannot insmod.

  The error log is:[ 5.415362] apex: loading out-of-tree module taints kernel.
[ 5.421347] Unable to handle kernel NULL pointer dereference at virtual address 00000003
[ 5.429094] Mem abort info:
[ 5.431854] Exception class = DABT (current EL), IL = 32 bits
[ 5.437745] SET = 0, FnV = 0
[ 5.440773] EA = 0, S1PTW = 0
[ 5.443892] Data abort info:
[ 5.446741] ISV = 0, ISS = 0x00000006
[ 5.450561] CM = 0, WnR = 0
[ 5.453512] user pgtable: 4k pages, 39-bit VAs, pgd = ffffffc046356000
[ 5.460007] [0000000000000003] *pgd=00000000c69d2003, *pud=00000000c69d2003, *pmd=0000000000000000
[ 5.468928] Internal error: Oops: 96000006 [#1] SMP
[ 5.473765] Modules linked in: apex(O+)
[ 5.477583] CPU: 3 PID: 689 Comm: insmod Tainted: G O 4.14.34-rt27+g5b7d979 #2
[ 5.485892] Hardware name: Freescale S32V234 (DT)
[ 5.490570] task: ffffffc0469a4280 task.stack: ffffff8009c68000
[ 5.496469] PC is at apex_probe+0x24/0x3d8 [apex]
[ 5.501143] LR is at apex_probe+0x24/0x3d8 [apex]
[ 5.505814] pc : [<ffffff80005f02b4>] lr : [<ffffff80005f02b4>] pstate: 20000145

0 项奖励
回复
4,942 次查看
nxa13002
NXP Employee
NXP Employee

Did you rebuild VSDK drivers ? . You need to rebuild VSDK drivers after you build Image and dtb

0 项奖励
回复
4,941 次查看
zhangweikanghus
Contributor III

Thank you I didn't rebuild it. I will try it soon.

0 项奖励
回复