How can I find and install S32G (S32G274A) SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I find and install S32G (S32G274A) SDK

4,778 Views
tiancy
Contributor I

I want to create a S32G274A application project in S32DS.

But I can`t find S32G274A  SDK in S32DS ( Project wizard  or Extensions & Updates).

How can I find and install S32G SDK ?

image.png

0 Kudos
6 Replies

3,803 Views
jeffin_joys
Contributor I

Hello,

Is there any latest S32G SDK available which can be integrated to S32 IDE?

Thanks

0 Kudos

3,779 Views
mikedoidge
NXP Employee
NXP Employee

Hello @jeffin_joys ,

Please see the document https://www.nxp.com/downloads/en/application-software/S32G2SWSS.pdf for the details on the latest SW offering on S32G.

Best Regards,

Mike

0 Kudos

4,562 Views
mikedoidge
NXP Employee
NXP Employee

Hello tiancy‌,

You need to go to https://nxp1.sharepoint.com/teams/ext566 and request an entitlement to gain access to the SDK download.

Best Regards,

Mike

0 Kudos

3,586 Views
lily95
Contributor I

Hello Mike:

Where can i request the entitlemnt t ogain the access of SDK download? THANKS@Mike

0 Kudos

3,566 Views
mikedoidge
NXP Employee
NXP Employee

Hello @lily95,

The delivery method for the S32G run-time software has changed. The Real-Time Drivers (RTD) package is available through the Automotive Software Package Manger.

Please note, there is both standalone and S32 Design Studio-integration packages available.

Best regards,

Mike

0 Kudos

3,548 Views
lily95
Contributor I

Hello Mike:

Thanks for the suggestion.

And i noticed i have to waiting for the approval of export Control, do you know how many days it may costs to get the approval?

Best regards,

lily

0 Kudos