How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How I can use CMSIS in S32K Design Studio with S32K148(freeRTOS)

2,901件の閲覧回数
Learner
Contributor III

Hi 
Is it possible to Integrate CMSIS with S32K Design Studio ?
If yes, Please share me the process to integrate CMSIS with S32K Design Studio.

Thanks 

0 件の賞賛
返信
2 返答(返信)

2,875件の閲覧回数
Learner
Contributor III

Thanks @mikedoidge 
I will go through with the tutorial.

0 件の賞賛
返信

2,886件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Learner,

There is a great tutorial on using CMSIS here: https://mcuoneclipse.com/2013/02/14/tutorial-using-the-arm-cmsis-library/

It was written by our colleague @BlackNight. While the device is different and the tool (CodeWarrior) is different, the steps should be quite similar as the devices use ARM cores and the tools are built on Eclipse.

Best Regards,

Mike

0 件の賞賛
返信