Generated files are referring headers from SDK in installing folder.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generated files are referring headers from SDK in installing folder.

ソリューションへジャンプ
1,962件の閲覧回数
tejo2one
Contributor III

I am using MPC5748G development kit with S32DS., new project is created by selecting create from example the generated files are referring header files from installing folder instead of project folder.

Any changes made to project folder are not being reflected to project instead header files in installing location are being reflected to project.

As a work around header included as following:

tejo2one_0-1677739401547.png

 

Please let me know if there is permanent solution.

 

0 件の賞賛
返信
1 解決策
1,911件の閲覧回数
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,920件の閲覧回数
Markus_Schroeder
Contributor II

I found the updated link:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Use-SDK-based-example-code-as-st...

Actually, it seems, the link was correct, only the 4 at the end was not interpreted as part of it.

0 件の賞賛
返信
1,912件の閲覧回数
tejo2one
Contributor III

Thanks for response. I did little search and found it.

.PE file already contained generate mode as "standalone".

I just removed include paths which were pointing to "c-drive" in "properties/Paths and Symbols/Includes".

After update:

tejo2one_0-1678117791185.png

 

0 件の賞賛
返信
1,943件の閲覧回数
jiri_kral
NXP Employee
NXP Employee
0 件の賞賛
返信
1,932件の閲覧回数
tejo2one
Contributor III

Thanks for response, page is no longer available.

Can you please check & reshare?

tejo2one_0-1678011623989.png

 

0 件の賞賛
返信