GHS compiler and S32 Design Studio for Arm 2018.R1

cancel
Showing results for 
Search instead for 
Did you mean: 

GHS compiler and S32 Design Studio for Arm 2018.R1

756 Views
Contributor I

hello,

now I'm trying to make a project with S32 Design Studio with below environment.

- MCU: S32k 146

-Compiler: Greenhils v2017.1.4

but I could not find the compiler setting on S32 Design Studio, only I could make a GCC project.

Do I need to install the plug-in for that? If yes, where can I find the material?

1 Reply

9 Views
NXP Employee
NXP Employee

Hi, 

please check this thread GHS plug-in can NOT successfully installed in S32DS for Power Architecture version 2017.R1 

You can contact Green Hills support to obtain toolchain plugin compatible with Eclipse Neon version (S32DS is based on Eclipse Neon). 

Hope it helps. 

Jiri