SW32R41_AZ_2.7.2_0.9.0_D2208__User_Manual.pdf.
4 How to Run and Debug an Application.
It only show how to Flash and Run the Application via Lauterbach TRACE32.
I don't have the Lauterbach, what I have is only a S32 Debugger.
I tried to flash and dubbug a Zephyr application elf or bin via S32 Debugger.
But when I download the elf file into S32R41 ram, the UART show:
*** Booting Zephyr OS build 40efdf68e768 ***
And then it pause and cannot proceed.
When I click the Resume button in S32 Design Studio 3.5, it only stop in the line:
0000000033c011b4: hlt #0x0
So, how to debug a zephyr APP elf via S32 debugegr?
And how to flash a zephyr APP bin into the flash and run it?
Hello Shawn,
Unfortunately, Zephyr OS is not yet supported by S32 Debugger. We do plan to add this support later this year. For now, you will need to use another debugger.
Also, please do not title your post with a name that resembles an instruction article from us. Unless you are providing the instructions this only creates confusion and frustration for other community members.
Best Regards,
Mike