Failed to load PFE firmware to S32G-VNP-EVB (S32G274A)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to load PFE firmware to S32G-VNP-EVB (S32G274A)

1,552 Views
toannnt
Contributor I

Hello, 

I am using S32G-VNP-EVB (S32G274) running Autosar basic software. 

The MCAL using in this platform is "eb-tresos-S32G2x_MCAL44_100_HF3_LLCE_PFE"

I am trying to enable the PFE Ethernet by calling Init function. 

However, the MCU running into exception due to bus error.

Reason: When loading PFE firmware, MCU accesses to PFE CBus base address ( PFE_CFG_CBUS_PHYS_BASE_ADDR_CPU  = 0x46000000). 

This address is not available/visible in Trace32 and causing bus error.

My question: 

Is there any specific procedure / configuration need to be done so that PFE memory address can be available ? 

Thanks

Tags (3)
0 Kudos
Reply
0 Replies