I try to install SW32k3 development package from SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite(help-install newsoftware),and the warning below will always pop up:
then i click"install anyway".The S32 DS IDE will close itself. When i tried to start it again, i found that the s32ds.exe file under "eclipse" is missing and i have to re-install S32DS v3.5
I also tried to update IDE with SW32K3_S32DS_3.5.13_D2407,still not working
Can anyboby help me with this issue?
PS.
installation details:
Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.0; Build id: 202207261752
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.0; Build id: 202207261752
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Hi
On some machines doesn't work repositories with http:// - please try to change http:// to https://
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
thanks a lot for your reply, i have change it as below:
but still not working. I tried to update the packages below, but the IDE close itself again with this pop up:
PS.
I have installed S32DS_ARM_v2018.R1 for the development for other projects. I don't know if it has anything to do with my problem
Best Regards