I try to install SW32k3 development package from SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite(help-install newsoftware),and the warning below will always pop up:

then i click"install anyway".The S32 DS IDE will close itself. When i tried to start it again, i found that the s32ds.exe file under "eclipse" is missing and i have to re-install S32DS v3.5

I also tried to update IDE with SW32K3_S32DS_3.5.13_D2407,still not working
Can anyboby help me with this issue?
PS.
installation details:
Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.0; Build id: 202207261752
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.0; Build id: 202207261752
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
S32K3S32DS-S32PLATFORM