Fail to install S32k3 development package to S32DS v3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fail to install S32k3 development package to S32DS v3.5

1,726件の閲覧回数
ErinYu
Contributor I

I try to install SW32k3 development package from SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite(help-install newsoftware),and the  warning below will always pop up:

ErinYu_0-1735176983912.png

 

 

then i click"install anyway".The S32 DS IDE will close itself. When i tried to start it again, i found that the s32ds.exe file under "eclipse" is missing and i have to re-install S32DS v3.5

ErinYu_1-1735176983966.png

 

I also tried to update IDE with SW32K3_S32DS_3.5.13_D2407,still not working

Can anyboby help me with this issue?

 

PS.

installation details:

Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.0; Build id: 202207261752
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.0; Build id: 202207261752
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521

S32K3S32DS-S32PLATFORM 

0 件の賞賛
返信
6 返答(返信)

1,705件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

On some machines doesn't work repositories with http:// - please try to change http:// to https://

Available S32DS Software Sites https.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,700件の閲覧回数
ErinYu
Contributor I

Hi,

thanks a lot for your reply, i have change it as below:

ErinYu_0-1735192473929.png

but still not working. I tried to update the packages below, but the IDE close itself again with this pop up:

 

ErinYu_2-1735192612392.png

 

PS.

I have installed S32DS_ARM_v2018.R1 for the development for other projects. I don't know if it has anything to do with my problem

Best Regards

 

 

0 件の賞賛
返信

1,694件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport
Have you tried to install S32K3 RTD 5.0.0 offline? Please refer to: HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 13 for S32DS: SW32_S32DS_3.5.13_D2407.zip
3. Install development package for S32K3XX: SW32K3_S32DS_3.5.13_D2407
4. Install development package for S32K396: SW32K39x_S32DS_3.5.13_D2407.zip
5. Install development package for S32M276: SW32M2_S32DS_3.5.13_D2407
6. Install updatesite for this release: SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.
zip
0 件の賞賛
返信

1,665件の閲覧回数
ErinYu
Contributor I

Please refer to the screenshot below:

ErinYu_0-1735195226004.pngErinYu_1-1735195240550.png

 

 

0 件の賞賛
返信

1,340件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please make sure that you updated PE Micro plugin to latest version - v3.5.9

0 件の賞賛
返信

1,691件の閲覧回数
ErinYu
Contributor I
Yes i tried. I tried install SW32_S32DS_3.5.13_D2407.zip but the progress stuck at 80% and the software closed itself again and s32ds.exe missed just as before
0 件の賞賛
返信