Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error when generating code for SCST Lib with S32K116, SDK 2.9.2 and IAR 8.22.2 c

1,624 次查看
tminh
Contributor I

Hello,

S32DS failed to generate SCST Library code with SDK S32K1xx_BETA_2.9.2 and IAR 8.22.2 compiler with below Error:

Description:   

Generator: FAILURE: at line 86: Unknown macro: "PE_G_XLKR_COMPILER" (file: Drivers\S32K\S32K144_SDK01\SCST.drv)

Location: scst2

Type: Processor Expert Problem

I could generate SCST successfully when not using IAR compiler.

Please help me to clarify this issue.

Thanks and Regards,

Minh

0 项奖励
回复
0 回复数