Error downloading to the device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error downloading to the device

1,518 Views
rkkhandekar55
Contributor I

Hiii

I am using S32 Design Studio version 1.2 IDE and PE-MICRO Debugger(openSDA) for S32K144 Eval board. I am trying to debug but every time I tried to load program, I receive an error as following

Error enabling module just selected.

Error loading programming algorithm - load aborted.

Error occured during Flash programming.

 

 

WARNING - NO RESET SCRIPT FILE HAS BEEN CONFIGURED TO RUN!!!

TO MODIFY THE RESET SCRIPT SETTINGS, USE THE FOLLOWING MENU OPTION:

CONFIGURATION -> AUTOMATED SCRIPT OPTIONS

 

PE-ERROR: Error downloading to the device.

How to solve this problem ?

Thanks in advance

Rahul

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,370 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS for ARM v1.2 is very old one. Please try to use latest release with fixed bugs - https://community.nxp.com/docs/DOC-340190 

Jiri

0 Kudos
Reply