Error compiling powerpc-eabivle-gcc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error compiling powerpc-eabivle-gcc

2,327 次查看
jfrey
Contributor IV

Compiling using the included instructions fails here:

Building eabi newlib
 401 config ...Ok
 402 build ...Ok
 403 install ...Ok
 404 install html ...Ok
 405 install pdf ...Error
标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,844 次查看
alexanderfedoto
NXP Employee
NXP Employee

Hello Jed

You can check log file in opt/freescale/ELe200/logs/install.405 for errors. Usually it happens when "texlive" pkg is not installed.

0 项奖励
回复

1,844 次查看
jfrey
Contributor IV

I have it installed. 

  1. Is there a way to cache and not wipe out intermediate steps? Every ./build restarts from extracting the base files. It makes debugging time consuming.
  2. I realise it's building docs, but does a compiler really need texlive to compile?
  3. Internally how much time has been spent trying to maintain this eclectic collection of versions software and 4674 line build script? Wouldn't it have been easier to just write an llvm backend? Then you could even keep the source to yourself. (BSD vs GPL).

I'm fairly apt at debugging and getting things compiled and running but this is a spaghetti heap of scripts and dependencies. 

0 项奖励
回复

1,844 次查看
alexanderfedoto
NXP Employee
NXP Employee

1. You can adjust dLSTSTEPS section in e200 build job descriptor. See in f-job/ELe200

Or you can set explicitly run

./build.sh s=F494 -s Ebin ELe200

where Ebin is desired step.

2 & 3. The build script has the same goal as ABE in Linaro environment.

0 项奖励
回复