Error S32K116_SDK_3.0.0_PATH for the Project is not found in SDKs list!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error S32K116_SDK_3.0.0_PATH for the Project is not found in SDKs list!

Jump to solution
2,574 Views
chaitanya_kalyani
Contributor III

Hello, 

 
 
 
 

Getting below error when I open project which is created by one of the my senior. Checked for IDE updates but no pending updates and not able to resolve the error. 

 

When I open project in S32 Design Studio for Arm 2018.R1 getting below error 

 

1.JPG

 

and when project is opened in S32 Design Studio for Arm 2.2 getting below error 

 

2.JPG

 

How to resolve this error. 

 

Thank you in advance.

 

Tags (1)
0 Kudos
1 Solution
2,545 Views
stanish
NXP Employee
NXP Employee

Hello, I suspect The project you are trying to open was created in some pre-release (EAR 1.8.7) version of SDK. 

1) I'd suggest you to create a new SDK project for S32K116 (latest RTM version is 3.0.3)

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2-2-Update-1...

2) add all the SDK components + setup from the original project

3) finally transfer all the non-generated source files. I suspect this will also require some adjustments on API level since there might be some changes between EAR vs. RTM releases of SDK.

 

If you intend on using the original project with the same SDK (1.8.7) you probably need to install S32DS for ARM 2018.R1 + Update 1 (https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2018-R1-Upda...)

Hope it helps,

Stan

 

View solution in original post

4 Replies
2,546 Views
stanish
NXP Employee
NXP Employee

Hello, I suspect The project you are trying to open was created in some pre-release (EAR 1.8.7) version of SDK. 

1) I'd suggest you to create a new SDK project for S32K116 (latest RTM version is 3.0.3)

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2-2-Update-1...

2) add all the SDK components + setup from the original project

3) finally transfer all the non-generated source files. I suspect this will also require some adjustments on API level since there might be some changes between EAR vs. RTM releases of SDK.

 

If you intend on using the original project with the same SDK (1.8.7) you probably need to install S32DS for ARM 2018.R1 + Update 1 (https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2018-R1-Upda...)

Hope it helps,

Stan

 

2,567 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you updated your S32DS installation? Anyway, the latest version of S32DS is https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-ARM-2-2-Windows-... with included S32 SDK RTM v3.0.0

0 Kudos
2,558 Views
chaitanya_kalyani
Contributor III

Hello @jiri_kral 

 

Thank you for quick response.

 

I already updated IDE with all updates.

 

When open project in S32 Design studio first I am getting 

 
 
 

3.JPG

 

after selecting "Yes To All" getting  

Screenshot (7).png

after selecting yes getting  

Screenshot (6).png

 

after selecting and compiling the program getting error 

5.JPG

 

 

0 Kudos
2,563 Views
chaitanya_kalyani
Contributor III

Hello @jiri_kral 

 

I already updated IDE with all updates.

0 Kudos