Download S32 DS for MPC57xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download S32 DS for MPC57xx

2,604 Views
bastian_schick
Contributor IV

Hi,

 

where can I download the S32 design studio for PowerPC VLE?

All links bring me to the ARM version.

 

Actually I search a GCC with VLE support.

 

Thanks for any hint

7 Replies

2,010 Views
stanish
NXP Employee
NXP Employee

Hi all

Please check the download section of S32 Design Studio. S32DS Power v1.1 should be back and available for download.

S32 Design Studio IDE|NXP 

Stan

2,010 Views
malekben
Contributor II

Thank you Stan.

Could you tell us what did you correct in the Tool ?

Why it keeps the same version ?

Regards,

Malek.

0 Kudos
Reply

2,010 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

compiler team find some bud in S32DS for power. They are fixing the bug now. S32DS will be available after the bug will be fixed. Please be patient.

Regards,

Martin

2,010 Views
anon-7914f51b36
Contributor I

Hi Martin,

Do you have some ETA on when it will be available again. Also, can an older version be used in the meantime?

Regards,

Teodor

2,010 Views
martin_kovar
NXP Employee
NXP Employee

Hello Toedor,

unfortunately, I do not know, when S32DS will be returned to NXP website. If you have installed or downloaded older version, you can definitely use it. But be careful about project portability. If you try to move project from S32DS v.1.0 workspace to S32DS v. 1.1 workspace, it will not work (there are changes in makefile paths).

I will contact my colleague today and ask him about any news regarding S32DS v 1.1. I hope it will be resolved soon.

Regards,

Martin

2,010 Views
bastian_schick
Contributor IV

Martin,

actually, I do not care for S32DS. I use Emacs and Make. So no need for Eclipse ;-)
But what I need is a GCC which supports VLE.

So it would be great if NXP would put the GCC on the web to download. Separate from S32DS.

Cheers

42Bastian

2,010 Views
malekben
Contributor II

Same for me.

0 Kudos
Reply