Do not automatically generating platform and rtos folders in the SDK folder?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do not automatically generating platform and rtos folders in the SDK folder?

933件の閲覧回数
jason_zhong0224
Contributor I

Hi,

OS: Win10

IDE:  S32 Design Studio for ARM Version 2018.R1

Board: S32K144 chip

The questions are as follows:

Due to business needs, we adjusted the location of files in the SDK folder and created an NXP folder to store and manage these files

As shown in the picture below

jason_zhong0224_1-1672882117436.png

 

However, when the project is imported using S32, the platform and rtos folders are automatically regenerated. The final compilation results in an error

jason_zhong0224_2-1672882117014.png

 

Can you help me?

0 件の賞賛
返信
1 返信

906件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Jason,

Unfortunately, it is not possible to change to location of where the generated files are placed.

There is a similar thread on this topic:

is it possible to change S32DS generated code directory?

Perhaps you could change the include paths to ignore the generated folders and add a pre-compile script to copy the generated files into the location you've selected.

Best Regards,

Mike

0 件の賞賛
返信