Could not connect to semihosting port due to connection timeout. Please check that the correct port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not connect to semihosting port due to connection timeout. Please check that the correct port

3,856 Views
p_decesare
Contributor III

Hi, I  have a problem. My code doesn't work because on the console I have this problem:

 

Could not connect to semihosting port due to connection timeout. Please check that the correct port number is configured.

How could I repair this problem?

My code worked perfectly, but now I have this problem.
Can someone help me?

 

Thanks 

Best regards,

Paola

3 Replies

2,181 Views
Drifter22
Contributor II

Same problem for me with v.3.5. All has worked until yesterday, then today this error appears.

0 Kudos
Reply

3,826 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS Version and MCU? 

 

Jiri

0 Kudos
Reply

2,822 Views
steven_zhang
Contributor V

i have the same problem  ,S32DS3.4    P32K344EHVPBS1P55A  

0 Kudos
Reply