Hi,
I try to make my own SPI initialization without using SDK (for an internship).
I wrote a API in order to initialize a Slave but I can't receive frames. 
Anyone know out to initialize a Slave with registers please ? 
Fred
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
Could you please provide the project you created? It is difficult to know what could be the issue from the details you have provided. There are many things which could cause the slave to not receive the frames, it is hard to guess which could be the cause.
Mike
Hi and thank you for your reply.
Here my project.
DriverSPI_t spi0 = {
 .driver_SPI = LPSPI0,
 .speed = 9600,
 .Frame_Size = 15u,
 .mode_SPI = SPI_Mode_Master ,
 .cpol = SPI_Clock_Polarity_Enable_low,
 .cpha = SPI_Clock_Phase_Leading_Edge,
 .IsLSBFirst = SPI_Data_MSB_First,
 .spi_pcs = SPI_PCS_1,
 .pin_pcs = 31, //PTA31
 .pin_sck = 2,
 .pin_sin = 3,
 .pin_sout = 1,
 .port = PORTB
      };
DriverSPI_t spi2 = {
 .driver_SPI = LPSPI2,
 .speed = 9600,
 .Frame_Size = 31u,
 .mode_SPI = SPI_Mode_Slave,
 .cpol = SPI_Clock_Polarity_Enable_low,
 .cpha = SPI_Clock_Phase_Following_Edge,
 .IsLSBFirst = SPI_Data_MSB_First,
 .spi_pcs = SPI_PCS_2,
 .pin_pcs = 13,
 .pin_sck = 15,
 .pin_sin = 16,
 .pin_sout = 8, //A8
 .port = PORTE
   };
void spi_init(DriverSPI_t spi){
 if(spi.driver_SPI == LPSPI0)
 {
 PCC->PCCn[PCC_LPSPI0_INDEX] = 0;
 PCC->PCCn[PCC_LPSPI0_INDEX] = Clock_Launch_SPI; //Activation of the SPI clock
 }
 else if(spi.driver_SPI == LPSPI1){
 PCC->PCCn[PCC_LPSPI1_INDEX] = 0;
 PCC->PCCn[PCC_LPSPI1_INDEX] = Clock_Launch_SPI; //Activation of the SPI clock
 }
 else if(spi.driver_SPI == LPSPI2){
 PCC->PCCn[PCC_LPSPI2_INDEX] = 0;
 PCC->PCCn[PCC_LPSPI2_INDEX] = 0xC6000000; //Activation of the SPI clock
 }
spi.driver_SPI->CR = LPSPI_CR_RST_MASK;
 spi.driver_SPI->CR = 0x00000000 ; //Disable module
if(spi.mode_SPI == SPI_Mode_Master){ //Init Master mode
 spi.driver_SPI->IER = LPSPI_IER_TDIE(1) | LPSPI_IER_RDIE(1) ; //Receive and transmit data interrupt enabled
 spi.driver_SPI->DER = 0 ;
 spi.driver_SPI->CFGR0 = 0 ;
 spi.driver_SPI->CFGR1 = LPSPI_CFGR1_MASTER(spi.mode_SPI) |
 LPSPI_CFGR1_SAMPLE(0) |
 LPSPI_CFGR1_AUTOPCS(0) |
 LPSPI_CFGR1_NOSTALL(0) |
 LPSPI_CFGR1_PCSPOL(2) | //All peripheral chip select pin is active high
 LPSPI_CFGR1_MATCFG(0) |
 LPSPI_CFGR1_PINCFG(0) |
 LPSPI_CFGR1_OUTCFG(0) |
 LPSPI_CFGR1_PCSCFG(0);
 spi.driver_SPI->TCR = LPSPI_TCR_FRAMESZ(spi.Frame_Size) |
 LPSPI_TCR_WIDTH(0) |
 LPSPI_TCR_TXMSK(0) |
 LPSPI_TCR_LSBF(MSB_First) |
 LPSPI_TCR_PCS(spi.spi_pcs) |
 LPSPI_TCR_PRESCALE(3) | //functional clock/Prescaler = 7MHz
 LPSPI_TCR_CPHA(spi.cpha) |
 LPSPI_TCR_CPOL(spi.cpol);
 spi.driver_SPI->CCR = LPSPI_CCR_SCKDIV(5u) | //SCK = 1Mhz, T=1µs
 LPSPI_CCR_DBT(8u) | //1.43µs between frame
 LPSPI_CCR_PCSSCK(4u) | //714.3 from the PCS assertion to the first SCK edge
 LPSPI_CCR_SCKPCS(4u); //714.3 from the last edge to the PCS negation
 spi.driver_SPI->FCR = LPSPI_FCR_TXWATER(3u) | //Transmit Data flag set when # words <= 3
 LPSPI_FCR_RXWATER(0u); //Receive Data flag set when # words > 0
 }
 else if(spi.mode_SPI == SPI_Mode_Slave){ //Init Slave mode
 spi.driver_SPI->IER = 0x00000000 ; //Receive and transmit data interrupt enabled
 spi.driver_SPI->DER = 0 ;
 spi.driver_SPI->CFGR0 = 0 ;
 spi.driver_SPI->CFGR1 = LPSPI_CFGR1_MASTER(spi.mode_SPI) | //Slave mode
 LPSPI_CFGR1_SAMPLE(0) |
 LPSPI_CFGR1_AUTOPCS(1) |
 LPSPI_CFGR1_NOSTALL(0) |
 LPSPI_CFGR1_PCSPOL(1) | //Chip select 0 is active high
 LPSPI_CFGR1_MATCFG(0) |
 LPSPI_CFGR1_PINCFG(0) |
 LPSPI_CFGR1_OUTCFG(0) |
 LPSPI_CFGR1_PCSCFG(0);
 spi.driver_SPI->TCR = LPSPI_TCR_FRAMESZ(spi.Frame_Size) | //Size of the the frame
 LPSPI_TCR_WIDTH(0) |
 LPSPI_TCR_RXMSK(0) |
 LPSPI_TCR_LSBF(spi.IsLSBFirst) |
 LPSPI_TCR_PCS(spi.spi_pcs) |
 LPSPI_TCR_PRESCALE(2u) |
 LPSPI_TCR_CPHA(spi.cpha) |
 LPSPI_TCR_CPOL(spi.cpol);
 spi.driver_SPI->FCR = LPSPI_FCR_TXWATER(3u) | //Transmit Data flag set when # words <= 3
 LPSPI_FCR_RXWATER(0u); //Receive Data flag set when # words > 0
 }
spi.driver_SPI->CR = SPI_Launch; //Enable module
 if(spi.driver_SPI == LPSPI0){
 spi.port->PCR[spi.pin_sck] |= PORT_PCR_MUX(3u);
 spi.port->PCR[spi.pin_sin] |= PORT_PCR_MUX(3u);
 spi.port->PCR[spi.pin_sout] |= PORT_PCR_MUX(3u);
 if(spi.mode_SPI == SPI_Mode_Master){
 PORTA->PCR[spi.pin_pcs] |= PORT_PCR_MUX(4u);
 }
 }
 else if(spi.driver_SPI == LPSPI2){
 spi.port->PCR[spi.pin_sck] |= PORT_PCR_MUX(3u);
 spi.port->PCR[spi.pin_sin] |= PORT_PCR_MUX(3u);
 PORTA->PCR[spi.pin_sout] |= PORT_PCR_MUX(3u);
 if(spi.mode_SPI == SPI_Mode_Master){
 spi.port->PCR[spi.pin_pcs] |= PORT_PCR_MUX(2u);
 }
 }
}
--------------------------------
And here the polling mode to receive the frame.
while(!(LPSPI0->SR & LPSPI_SR_TDF_MASK) );
 LPSPI0->TDR = 0x1402;
 LPSPI0->SR |= LPSPI_SR_TDF_MASK;
while((LPSPI2->SR & LPSPI_SR_RDF_MASK)>>LPSPI_SR_RDF_SHIFT==0);
 receive_Frame_SPI = LPSPI2->RDR;
 }
Thanks by advance.
Fred
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Since some of your settings are hidden behind macros, it is hard know for sure. I think you have a couple of settings wrong.
spi.driver_SPI->CR = 0x00000000 ; //Disable module -> This should be enabled, set it to 0x00000001
and
spi.driver_SPI->CCR = LPSPI_CCR_SCKDIV(5u) | //SCK = 1Mhz, T=1µs -> This should be set to 8, not 5.
You also might find this useful: https://www.nxp.com/docs/en/application-note/AN5413.pdf
Best Regards,
Mike
Hi,
Yes I am sorry for that, i will put my program whitout the macro.
#define SPI_Launch 0x00000009
#define Clock_Launch_SPI 0xC6000000
#define MSB_First 0u
#define LSB_First 1u
typedef enum{
 SPI_Clock_Polarity_Enable_low = 0u,
 SPI_Clock_Polarity_Enable_high = 1u
} SPI_Clock_Polarity_t;
typedef enum{
 SPI_Mode_Slave = 0u,
 SPI_Mode_Master = 1u
} SPI_Mode_t;
typedef enum{
 SPI_Clock_Phase_Leading_Edge = 0u,
 SPI_Clock_Phase_Following_Edge = 1u
} SPI_Clock_Phase_t;
typedef enum{
 SPI_Data_MSB_First = 0u,
 SPI_Data_LSB_First = 1u
} SPI_LSB_First_t;
typedef enum{
 SPI_PCS_0 = 0u,
 SPI_PCS_1 = 1u,
 SPI_PCS_2 = 2u,
 SPI_PCS_3 = 3u
} SPI_PCS_t;
For the Control Register CR, I already saw on the Application note AN5413 that I have to disable the module in order to set the registers, and enable the module after that.
For the Clock Configuration Register CCR, I forgot to tell you that I used the S32K148 in HSRUN mode (The BUS_CLK is to 56MHz), so this is fine.
Again I am sorry, I don't use often forum when I have problems.
Fred.
 
					
				
		
 mikedoidge
		
			mikedoidge
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Fred,
This request is really about LPSPI on the S32K1xx family and nothing specific to S32DS. I strongly urge you to pursue this on the dedicated community for the S32K family of MCUs. https://community.nxp.com/community/s32/s32k
There is much information about SPI and how to program it. You can search the discussion threads and see what others have already done.
I would also suggest that you try using the SDK demo provided in S32DS as a way to verify that your hardware setup is good. This way you will know the issue remains just in your code.
Best Regards,
Mike
Sorry, for the IER register, it's equal to 0.