Clock configuration : MCU is not supported

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Clock configuration : MCU is not supported

跳至解决方案
2,053 次查看
Changwoo82
Contributor II

Hello!

I'm using the S32K3X8 Evaluation board.

Though I'm trying to change the clock division, it is failed because of error "MCU is not supported".

How can I solve this problem? 

 

 

0 项奖励
回复
1 解答
2,000 次查看
Changwoo82
Contributor II

It was caused by DRM in company.

it was resolved after decrypting the file 'S32V2xx.dsn.

 

Thank you.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,011 次查看
Changwoo82
Contributor II

Hello.

 

Thank you for answer. Unfortunately, I installed S32DS v3.5 and RTD for S32K358...

After posting this, I found the same issue with this. It was related with the DRM in laptop.

So, I need to check this point at first, then I'll get back.

0 项奖励
回复
2,035 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Which version of S32K3 RTD did you install for S32DS v3.5? Please install RTD that supports S32K358. What I installed is S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can change the clock division in the Clocks tool of S32CT.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,001 次查看
Changwoo82
Contributor II

It was caused by DRM in company.

it was resolved after decrypting the file 'S32V2xx.dsn.

 

Thank you.

0 项奖励
回复