Cannot install Configuration Tools on S32 Design Studio 3.6.0 for Ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot install Configuration Tools on S32 Design Studio 3.6.0 for Ubuntu

3,788 Views
jleveque
Contributor I

I am unable to install the "S32 Configuration Tools R1.8 NPI data package for S32K3" extension for S32 Design Studio 3.6.0 running on Ubuntu. I receive the error in the attached screenshot. Without the Configuration Tools installed, if I click on anything in the "ConfigTools" menu (E.g., "Pins", "Clocks," "Peripherals"), the IDE crashes from a segmentation fault. Please help me install the Configuration Tools on Ubuntu.

0 Kudos
Reply
8 Replies

3,671 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you installed S32K3xx RTD v5.0.0 ? The Config tool depends on it. 

0 Kudos
Reply

3,655 Views
jleveque
Contributor I

Where can I find "S32K3xx RTD v5.0.0"? I am developing for a S32K344 MCU, and if I look at what's available for the S32k344, the latest RTD is v3.0.0. If I search for S32K3, the latest is 4.0.0_P19 (see screenshot below).

RTD_offerings.png

0 Kudos
Reply

3,630 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can find it as an offline package in your software account

https://www.nxp.com/mynxp/profile

jiri_kral_0-1734534281345.png

 

0 Kudos
Reply

3,619 Views
jleveque
Contributor I

Thank you. I downloaded SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip and in S32 Design Studio, I added that zip file using the "Add Update Sites" option. However, I do not see any extensions show up in the "Available/Update" list. What do I need to do to install this?

0 Kudos
Reply

3,605 Views
jleveque
Contributor I

I found this post where you informed someone else that

RTD is not supported on Linux - but can be installed as an offline update package. The package can be download as a .zip archive from your NXP Downloads account. 

You can install it via Help -> Install New Software

So I tried this method, and I am greeted with the following error:

error.png

 

0 Kudos
Reply

2,883 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry, I missed that you are installing it on Ubuntu. Unfortunately RTD is not supported on Ubuntu host. 

0 Kudos
Reply

2,871 Views
jleveque
Contributor I

Thank you for the reply. That's unfortunate news, because S32 Design Studio is practically useless without RTD support. Does NXP have plans to add RTD support on Ubuntu hosts?

0 Kudos
Reply

2,789 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, there is a plan for full Linux support, but the exact date of release is not known yet. 

0 Kudos
Reply