Can we install S32DS 3.2 in Ubuntu 18.04?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can we install S32DS 3.2 in Ubuntu 18.04?

跳至解决方案
5,449 次查看
kiminkim
NXP Employee
NXP Employee

Hello, all

Is S32DS 3.2 supported in Ubuntu 18.04?

Guide manual only mentions Ubuntu16.04.

Do we need additional patch for installation?

Thank you

BR

Justin

标签 (1)
标记 (3)
1 解答
5,340 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Justin, 

Ubuntu 18.04 is not officially supported, but it is possible install S32DS on this version and use it. Please follow installation requirements for Linux host (java version 1.8, some 32 bit libraries and So on). 

Jiri 

在原帖中查看解决方案

7 回复数
5,341 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Justin, 

Ubuntu 18.04 is not officially supported, but it is possible install S32DS on this version and use it. Please follow installation requirements for Linux host (java version 1.8, some 32 bit libraries and So on). 

Jiri 

5,340 次查看
kiminkim
NXP Employee
NXP Employee

Hello, Jiri

When I tried to run S32DS 3.2 after installation I had a similar issue with this article:S32DS 3.2 fails to install on Ubuntu 18.04.4 with a weird Java complaint? 

I got this error log when loading bar almost reach to 50%.

justin@justin-PC:~/NXP/S32DS.3.2$ ./s32ds.sh
Jul 02, 2020 10:39:51 AM com.nxp.swtools.common.utils.runtime.SingletonProvider getSingletonInstance
SEVERE: getSingletonInstance for com.nxp.swtools.ivt.controller.IVTController
java.lang.reflect.InvocationTargetException
at sun.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method)
at sun.reflect.NativeConstructorAccessorImpl.newInstance(NativeConstructorAccessorImpl.java:62)
at sun.reflect.DelegatingConstructorAccessorImpl.newInstance(DelegatingConstructorAccessorImpl.java:45)
at java.lang.reflect.Constructor.newInstance(Constructor.java:423)
at com.nxp.swtools.common.utils.runtime.SingletonProvider.getSingletonInstance(SingletonProvider.java:46)
at com.nxp.swtools.common.ui.utils.swt.internal.SWTFactory.getSingletonInstance(SWTFactory.java:440)
at com.nxp.swtools.common.ui.utils.swt.SWTFactoryProxy.getSingletonInstance(SWTFactoryProxy.java:457)
at com.nxp.swtools.ivt.controller.IVTController.getInstance(IVTController.java:192)
at com.nxp.swtools.ivt.main.IVTServiceProvider.existsPointerOfLockState(IVTServiceProvider.java:48)
at com.nxp.swtools.ivt.main.IVTServiceProvider.getCurrentState(IVTServiceProvider.java:37)
at org.eclipse.ui.internal.services.EvaluationService.addSourceProvider(EvaluationService.java:157)
at org.eclipse.ui.internal.Workbench$47.runWithException(Workbench.java:2450)
at org.eclipse.ui.internal.StartupThreading$StartupRunnable.run(StartupThreading.java:32)
at org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:233)
at org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:145)
at org.eclipse.swt.widgets.Display.syncExec(Display.java:5414)
at org.eclipse.ui.internal.StartupThreading.runWithoutExceptions(StartupThreading.java:95)
at org.eclipse.ui.internal.Workbench.initializeDefaultServices(Workbench.java:2442)
at org.eclipse.ui.internal.Workbench.init(Workbench.java:1678)
at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2944)
at org.eclipse.ui.internal.Workbench.access$9(Workbench.java:2875)
at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:684)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:336)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:610)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:148)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:138)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:673)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:610)
at org.eclipse.equinox.launcher.Main.run(Main.java:1519)
at org.eclipse.equinox.launcher.Main.main(Main.java:1492)
Caused by: java.lang.NoClassDefFoundError: javafx/beans/property/SimpleBooleanProperty
at com.nxp.swtools.bootimage.settings.ABaseComponentSetting.<init>(ABaseComponentSetting.java:39)
at com.nxp.swtools.bootimage.settings.ABaseComponentSetting.<init>(ABaseComponentSetting.java:58)
at com.nxp.swtools.bootimage.settings.ImageHeader.<init>(ImageHeader.java:85)
at com.nxp.swtools.ivt.model.setting.IVTConfiguration.<init>(IVTConfiguration.java:100)
at com.nxp.swtools.ivt.mcu.EmptyMcu.getIvtConfiguration(EmptyMcu.java:151)
at com.nxp.swtools.ivt.controller.IVTController.<init>(IVTController.java:143)
... 39 more
Caused by: java.lang.ClassNotFoundException: Unable to locate JavaFX. Please make sure you have a JDK with JavaFX installed eg on Linux you require an Oracle JDK
at org.eclipse.fx.osgi.fxloader.FXClassLoader.postFindClass(FXClassLoader.java:64)
at org.eclipse.osgi.internal.loader.BundleLoader.searchHooks(BundleLoader.java:477)
at org.eclipse.osgi.internal.loader.BundleLoader.findClassInternal(BundleLoader.java:440)
at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:372)
at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:364)
at org.eclipse.osgi.internal.loader.ModuleClassLoader.loadClass(ModuleClassLoader.java:161)
at java.lang.ClassLoader.loadClass(ClassLoader.java:351)
... 45 more

Job found still running after platform shutdown. Jobs should be canceled by the plugin that scheduled them during shutdown: org.eclipse.jdt.internal.ui.InitializeAfterLoadJob

And here is how I solved this issue:

Main point was that I had to run with java SDK provided by Oracle.

1. Download "jdk-8u251-linux-x64.tar.gz" from Java SE Development Kit 8 - Downloads | Oracle 대한민국 by manual

2. Unzip and copy unziped folder to /usr/lib/jvm

tar -xvf ~/Downloads/jdk-8u251-linux-x64.tar.gz
sudo mkdir -p /usr/lib/jvm/jdk1.8.0_251
sudo mv jdk1.8.0_251/* /usr/lib/jvm/jdk1.8.0_251/

3. Add jdk1.8.0 to lists of java

sudo update-alternatives --install "/usr/bin/java" "java" "/usr/lib/jvm/jdk1.8.0_251/bin/java" 2048
sudo update-alternatives --install "/usr/bin/javac" "javac" "/usr/lib/jvm/jdk1.8.0_251/bin/javac" 2048
sudo update-alternatives --install "/usr/bin/javaws" "javaws" "/usr/lib/jvm/jdk1.8.0_251/bin/javaws" 2048

4. Choose jdk1.8.0 that we installed. type '2' in this case.

justin@justin-PC:~$ sudo update-alternatives --config java
There are 2 choices for the alternative java (providing /usr/bin/java).

Selection Path Priority Status
------------------------------------------------------------
0 /usr/lib/jvm/jdk1.8.0_251/bin/java 2048 auto mode
* 1 /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java 1081 manual mode
2 /usr/lib/jvm/jdk1.8.0_251/bin/java 2048 manual mode

Press <enter> to keep the current choice[*], or type selection number:

5. Confirm if it is applied properly.

justin@justin-PC:~$ java -version
java version "1.8.0_251"
Java(TM) SE Runtime Environment (build 1.8.0_251-b08)
Java HotSpot(TM) 64-Bit Server VM (build 25.251-b08, mixed mode)

In my previous setting which S32DS doesn't work, this is version that I have:

justin@justin-PC:~$ java -version
openjdk version "1.8.0_252"
OpenJDK Runtime Environment (build 1.8.0_252-8u252-b09-1~18.04-b09)
OpenJDK 64-Bit Server VM (build 25.252-b09, mixed mode)

After all this workaround, I can run S32DS well now.

Let me update more once I find another issue.

Thank you

BR

Justin

4,187 次查看
sateesh_kalidas
Contributor II

Thank you @kiminkim . I also had to make sure that JAVA_HOME is pointing to the correct directory in my .bashrc.

Regards

Sateesh

 

0 项奖励
4,718 次查看
suly-texas
Contributor I

Is it possible for you to email me a copy of that compressed file "jdk-8u251-linux-x64.tar.gz". I can order you the biggest pizza for your help?

sulanka@gmail.com

0 项奖励
4,704 次查看
E-John
Contributor III

Hi Sulanka,

 

This could be download from the following link,

https://www.oracle.com/tw/java/technologies/javase/javase8u211-later-archive-downloads.html

 

Best regards,

E-John

4,800 次查看
E-John
Contributor III

this works for me too (run S32 Design Studio IDE 3.4 on Ubuntu 18.04)

0 项奖励
3,800 次查看
manu23319
Contributor I

Hi, 

I tried to install S32 IDE on ubuntu 18.04 b but installation is stuck at license activation window, even I entered valid license key

0 项奖励