Can't install TCPIP 1.0.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't install TCPIP 1.0.3

5,149 Views
cw20
Contributor II

Hi,

I cannot install TCPIP v1.0.3 onto DS 3.5. I installed all the required packages and the correct versions. I've tried adding it through the extension and updates window as well as the "install new software" option but both do not work. As a result, the lwip example is not available. What should I do?

 

I've included all the packages I have installed in a txt file.  

Tags (3)
0 Kudos
Reply
5 Replies

5,093 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cw20 ,

Please ca you share the Workspace installation log to understand the issue. 

From Path

C:\Users\Public\[Woskapce_name]\.metadata 

(or wherever your workspace is located. 

Thank you. Best regards. 

- Mehul Patel

 

0 Kudos
Reply

4,597 Views
shunyizhang
Contributor IV

Hi @Mehul_Patel_NXP ,

any updates on how to fix this issue?

0 Kudos
Reply

5,073 Views
cw20
Contributor II

Hi @Mehul_Patel_NXP 

Here's the workspace installation log. Thanks

0 Kudos
Reply

5,031 Views
cw20
Contributor II

Hi @Mehul_Patel_NXP ,

any updates on how to fix this issue?

0 Kudos
Reply

5,018 Views
bwp530
Contributor IV

same issue

0 Kudos
Reply