Can not open S32 configuration tool in S32 DS 3.4 for S32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not open S32 configuration tool in S32 DS 3.4 for S32k144

1,546 Views
sh_comm
Contributor I

I installed S32 Design studio 3.4 on ubuntu and make project for S32K144.

and I try to use s32 configuration tool for pin or peripherals but tool shows errors following capture image. network works well.  How can I resolve it?

 

s32_config_error.jpg

 

 

 

0 Kudos
Reply
1 Reply

1,477 Views
mikedoidge
NXP Employee
NXP Employee

You are getting this error message because you are missing some required component. For best user experience, we recommend all S32 Design Studio users to install additional NXP-developed packages using the S32DS Extensions and Updates menu. This menu can be opened from: Help -> S32DS Extensions and Updates. To resolve the issue, please ensure you have the following packages installed:

1) S32K1xx development package v3.4.1
2) Either S32SDK S32K1XX RTM 4.0.2
OR RTD S32K1 1.0.0

S32DS Extensions and Updates S32K1xx.png

Best regards,

Mike

0 Kudos
Reply