Built Binarry File 0x00 -> 0xFF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Built Binarry File 0x00 -> 0xFF

310件の閲覧回数
pyi285
Contributor II

If you build it as a binary file or elf file and open the files, it says 0x00. A picture is also attached to the link below. So, as described below
#pragma fill_alignment_data_with_FF on
I'm trying to put it, but I don't know exactly where to put it.
I think I put everything in there.
can you solve it

1. When I open a binary file or an elf file, the 0xFF part is 0x00.
2. #pragma fill_alignment_data_with_FF on where to put the code source

https://community.nxp.com/t5/MPC5xxx/Firmware-and-bootloader-binary-file-issues/m-p/1674859#M23855

 

#bootload #mpc5674F #SPC5674F #MPC

0 件の賞賛
返信
0 返答(返信)