Building S32K146 project in S32DS from command line can't find library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building S32K146 project in S32DS from command line can't find library

2,230 次查看
tommy1231
Contributor II

I'm trying to build an S32K146 project in the S32DS 2.2 and it can't find a library

c:/nxp/s32ds_arm_v2.2/s32ds/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: cannot find -l:S32K14x_AMMCLIB.a

If I build the same project within the S32DS it builds correctly.

The library search path is set to

"${S32K14X_AMMCLIB_1.1.18_PATH}/lib/s32ds_arm32"

If I change this to point directly to it

C:\NXP\S32DS_ARM_v2.2\S32DS\software\AMMCLIB_v1.1.18\S32K14x_AMMCLIB_v1.1.18\lib\s32ds_arm32

Then it builds from the command line.

This is the command I'm using from the command line

eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Users\christom\workspaceS32DS.ARM.2.2_cmd -import C:\Users\christom\HED-MCU-Workspace\PM-04J-S32K -build PM_04J_S32K/App_Debug --launcher.suppressErrors

Looking for the best way to resolve

标记 (4)
0 项奖励
回复
2 回复数

2,164 次查看
ErichStyger
Specialist I

It seems to me that it cannot resolve/find the variable S32K14X_AMMCLIB_1.1.18_PATH.

How did you define that variable? As CDT variable or in the workspace?

I did not try it, but maybe it works if you have that variable defined on console calling Eclipse?

0 项奖励
回复

2,164 次查看
tommy1231
Contributor II

I didn't define it, that was one of the default settings when S32DS created the project.  It can be found here in the linked resources

pastedImage_1.png

0 项奖励
回复