Building S32K146 project in S32DS from command line can't find library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building S32K146 project in S32DS from command line can't find library

2,354件の閲覧回数
tommy1231
Contributor II

I'm trying to build an S32K146 project in the S32DS 2.2 and it can't find a library

c:/nxp/s32ds_arm_v2.2/s32ds/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: cannot find -l:S32K14x_AMMCLIB.a

If I build the same project within the S32DS it builds correctly.

The library search path is set to

"${S32K14X_AMMCLIB_1.1.18_PATH}/lib/s32ds_arm32"

If I change this to point directly to it

C:\NXP\S32DS_ARM_v2.2\S32DS\software\AMMCLIB_v1.1.18\S32K14x_AMMCLIB_v1.1.18\lib\s32ds_arm32

Then it builds from the command line.

This is the command I'm using from the command line

eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Users\christom\workspaceS32DS.ARM.2.2_cmd -import C:\Users\christom\HED-MCU-Workspace\PM-04J-S32K -build PM_04J_S32K/App_Debug --launcher.suppressErrors

Looking for the best way to resolve

タグ(4)
0 件の賞賛
返信
2 返答(返信)

2,288件の閲覧回数
ErichStyger
Specialist I

It seems to me that it cannot resolve/find the variable S32K14X_AMMCLIB_1.1.18_PATH.

How did you define that variable? As CDT variable or in the workspace?

I did not try it, but maybe it works if you have that variable defined on console calling Eclipse?

0 件の賞賛
返信

2,288件の閲覧回数
tommy1231
Contributor II

I didn't define it, that was one of the default settings when S32DS created the project.  It can be found here in the linked resources

pastedImage_1.png

0 件の賞賛
返信