Build error in all programs including examples also

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build error in all programs including examples also

4,232 Views
RajG
Contributor III

help me i am stuck with this type of 5 error in any program even in examples, other examples gives first and second error different rest all errors as it is, please help. 

0 Kudos
Reply
3 Replies

4,204 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share output from build console? If it is working on another machine - try to re-install S32DS. 

 

Jiri

0 Kudos
Reply

4,197 Views
RajG
Contributor III

@jiri_kral thanks for the reply, I will attach build console screenshot below. I have tried to re-install the complete program also tried to update all its pack, but still it throws this errors.

I am using Windows 7 and it shows this error. Another Windows 10 system runs and build this program correctly, so my guess is windows 7 is having some issue.

Please help further...

Thanks and Regard,

Raj G.

0 Kudos
Reply

4,207 Views
RajG
Contributor III

I tried to install and run examples codes in another PC and it build correctly without any of errors so my guess is there is something strange with my other system.....

0 Kudos
Reply