Boot Rom execution stopped in S32R294 EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot Rom execution stopped in S32R294 EVB

959 次查看
HyunungPark
Contributor III

I want to boot from flash in S32R294 EVB.

But Boot Rom Code stops like below.

What should I do to issue this issue?

Starting reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&E\s32e200_s32r294.mac) ...
REM This script is compatible with S32R294 devices.
REM Clean GPRs to remove residual data after using algorithm
REM Initialize all of the Main DSRAM - 1024KB
Initializing RAM from $40000000 to $400FFFFF.
Initializing Ram Block 0x40000000-0x400FFFFF.

Reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&E\s32e200_s32r294.mac) completed.

Running Boot Rom ...
Initializing Ram Block 0x40000000-0x4000000F.
Stopping Boot Rom code. (Did not exit boot rom as expected)
Boot Rom execution stopped. (pc=0x00002048)
S32R294 Device detected

BRs.

Hyunung Park

0 项奖励
回复
1 回复

758 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @HyunungPark ,

 

Very sorry for checking this case very late. 

 

Please let us know if you were able to resolve the issue, if yes what was the problem. 

 

Thank you. Best regards. 

-Mehul Patel 

0 项奖励
回复