Availability of S32K3XX TCPIP STACK 1.0.3 D2306 Update Pack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Availability of S32K3XX TCPIP STACK 1.0.3 D2306 Update Pack

184 Views
noobsplzwin
Contributor I

Dear NXP Support Team,

I am currently developing a driver for the TJA1101BHN using the S32K3 platform. I came across a demo online that utilizes the S32K3XX TCPIP STACK 1.0.3 D2306 update pack, which seems to be perfectly suited for my project's requirements. However, I have searched through the NXP website and have not been able to find this specific update pack.

Could you please assist me in locating this update pack? If it is no longer available, or if there is a newer version that has replaced it.

Thank you very much for your support. 

Best regards,

Connor

0 Kudos
1 Reply

134 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Click S32K3 Standard Software ->Automotive SW - S32K3 - Stacks

Here you will find TCPIP STACK update pack.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos